CAN_CLK Setting in MBD for MPC57x 3.0 does not Match Data sheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN_CLK Setting in MBD for MPC57x 3.0 does not Match Data sheet

659 Views
abhishek_kumar1
Contributor IV

Dear All

For MPC5744P, the maximum CAN_CLK frequency must be 80MHz but the setting in mpc_clock_man_panther.c is 200MHz. Could you please explain this deviation?

Also, if I change the clock settings to 80MHz (using project to change the clock setting provided by NxP), the baudrate setting in the Simulink block Mask generates wrong code. 

I assume for the Simulink Block the input frequency is assumed to be 200MHz (as shown in the panther code comments) but i reality we shall only use maximum 80. To get the correct baudrate, I have to multiply the baudrate by 2.5. Which is not possible in the dropdown menu of Simulink block. 

Please provide a solution for this. 

pastedImage_2.png

pastedImage_3.png

pastedImage_1.png

rafael.barbosa@chassisbrakes.com

mariuslucianandrei

constantinrazvan.chivu

dumitru-daniel.popa

0 Kudos
1 Reply

561 Views
constantinrazva
NXP Employee
NXP Employee

Hello abhishek.kumar@chassisbrakes.com‌,

Sorry for the late reply - I'll take a look at this and provide a fix this week so you don't have to manually change the baudrate.

Kind regards,

Razvan.

0 Kudos