s32v :: auto-exposure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32v :: auto-exposure

Jump to solution
2,300 Views
18502532079
Contributor I

to whom may concern:

      hi, i am a engineer using s32v, i have a s32v-sbc board and a sony-imx224 camera which is recommended by nxp.

      i want to know if there are example codes to show whether s32v have the ability to auto-exposure imx224 camera.

                                                                                                                                                                                    ASAP

                                                                                                                                                                                 thank you!

Labels (1)
0 Kudos
1 Solution
2,162 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Andy,

We do have example graph for exposure control for imx224 sensor at s32v234_sdk\isp\graphs\imx224_exp_ctrl. But we don't have full fledged example in VSDK.

The complete exp control example is available for OV10640 sensor at s32v234_sdk\demos\isp\isp_ov10640_default. 

So you can take reference from isp_ov10640_default demo and port it to work with imx224 using imx224_exp_ctrl graph.

Regards,

Kushal

View solution in original post

0 Kudos
2 Replies
2,162 Views
paulvlase
NXP Employee
NXP Employee
kushalshah13

Do you know anyone that might be able to answer this question?

Thank you!

0 Kudos
2,163 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Andy,

We do have example graph for exposure control for imx224 sensor at s32v234_sdk\isp\graphs\imx224_exp_ctrl. But we don't have full fledged example in VSDK.

The complete exp control example is available for OV10640 sensor at s32v234_sdk\demos\isp\isp_ov10640_default. 

So you can take reference from isp_ov10640_default demo and port it to work with imx224 using imx224_exp_ctrl graph.

Regards,

Kushal

0 Kudos