mipi at 1.0V S32V234 eval

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mipi at 1.0V S32V234 eval

1,024 Views
sarawoo
Contributor I

on the s32v234 eval kit, the voltage of the mipi bus is called out at 1.0V.  i see you have camera - sony and ov cameras which use mipi at 1.2V.  i think the standard called out 1.2V as well.  is it OK for me to use the mipi interface on my sensor at 1.2v and connect it directly to the 1.0v mipi on the eval kit?  i think the dc component is removed, but want to confirm this is OK with NXP.

thanks!

Labels (1)
0 Kudos
1 Reply

919 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi kushalshah‌,

Do you know anyone that might be able to answer this question?

Thank you!

Daniel

0 Kudos