NXP FTF 2016 - 培训演示

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP FTF 2016 - Training Presentations

讨论

排序依据:
A look at new types of low- or battery-powered and space-constrained applications made possible be the latest innovations in communications processors, including portable storage, IoT Gateways and embedded control.
查看全文
This session will provide a detailed introduction to NXP's HomeKit Software Development Kit (SDK) architecture, APIs and code adaptors. Through hands-on examples, you will learn accessory profile configurations, how to integrate with accessory application software, and how to build and debug a demo accessory (Restricted to verified MFi licensees only).
查看全文
AC/DC converters need to provide a defined and safe supply voltage from AC mains, varying from 90 to 264 V AC. Key requirements are efficiency, no-load power consumption and size. A new requirement for wall chargers is communication to the mobile, enabling faster charging by changing voltage or current. Most common AC/DC topologies are flyback and resonant. A flyback converter features lowest cost, but magnetics size becomes larger at higher output power. In that case, resonant converters are preferred, although efficiency is lower at low loads. NXP has invented a resonant concept that overcomes this issue. The presentation will introduce the mentioned AC/DC technologies and NXP’s product advantages.
查看全文
Security is cited as one of the biggest obstacles preventing the IoT from reaching its potential. Learn how Trust Architecture in QorIQ processors can help you secure your IoT device, and provide end-to-end security for your IoT system - from the sensors to the cloud.
查看全文
Customers active in hospitality, home readers or any application connecting to a smartphone or tablet are faced with the challenge of guarantying system interoperability with all smartphones on the market today. The answer is given as an NFC and BLE turnkey solution - NXP’s NFC/BLE reference design (OM27462NBR) based on the PN7462 and the QN902x Bluetooth 4.0 Low Energy family.
查看全文
For drug delivery to be effective, two very important conditions need to be met. First, drug quality needs to be ensured until the time of administration to the patient. Second, the patient needs to adhere to the prescribed therapy. Two easy-to-use solutions will be presented. They comprise a battery, an antenna and a single chip that integrates a sensor, storage and NFC connectivity. Both solutions support wireless communication with a smart phone. A temperature monitoring solution permits logging of transport conditions of each individual drug package at any point in time. Patients and healthcare professionals can confirm the drug quality at the moment of administration. A therapy adherence monitoring solution for drug blisters and bottles records medication intake events. In case the intake deviates from prescription, patients can be reminded and motivated to do better.
查看全文
The modern car has already gone beyond a simple mode of transportation to a platform for connectivity. The challenges of balancing performance and cost have the new requirement to meet security as the car becomes connected to the rest of the world. This class will review the security implications for CAN communications. The class will walk through a hands-on connecting a CAN network of two MPC5748G devices via secure CAN communications. Leveraging the SHE firmware on the MPC5748G HSM. CAN messages with be signed before transmission and authenticated on the receiving end using CMAC and AES-128.
查看全文
NXP introducing the most comprehensive smart home/IoT Evaluation kit enabling multiple technologies as wireless connectivity, security & NFC commissioning with audio features. NXP's complete value proposition combines to give best user experience, performance and accuracy to develop best home/building automation solutions.
查看全文
This session will cover the basics of authentication for anticounterfeit applications. Topics covered include use cases and applications, hardware vs. software, symmetric vs. asymmetric crypto protocols, host and device requirements, attacks and countermeasures, and "beyond the chip" security concerns. An intro to the A1006 and A71 product families will also be provided.
查看全文
Transport ticketing requirements have evolved significantly over the last years - from transaction security to multi-application needs and the possibility to integrate mobile ticketing to an existing environment. NXP's MIFARE® products have consistently been able to meet these requirements and strongly establish an excellent reputation as the leading contactless solution delivering convenience, flexibility and scalability. Over 1,000 business partners including application developers, service and solution providers, system integrators and card manufacturers make up the open MIFARE community and ecosystem. MIFARE DESFire EV2 is the next-generation of MIFARE ICs with highest security level (EAL5+ Common Criteria certification) for hardware and software. Its enhanced key management makes it the ideal multi-application platform for unlimited applications.
查看全文
Learn about wireless trends and solutions for home, enterprise, industrial and infrastructure markets. Includes discussion on the QorIQ LS Series platform for 802.11ac, Kinetis platform for 802.15.4 and BLU for home and enterprise IoT control.
查看全文
Saving Space in your Reference Design with eSIM. eSIM (eUICC) and what it means for chipset makers and device OEMs. Today consumers want bigger screens, more battery life, more storage, more rich media content etc. The (R) evolution that eSIM will create is unique, disruptive and can be compared to the time when black and white TV went to Color. The OEMs are adopting slowly, but like the days of B&W TV, the networks weren’t ready, and neither are the Mobile operators in the case of eSIM!
查看全文
In this session, Linear Technology will provide detailed design guidelines for robust and scalable power solutions for the latest QorIQ processors. Using proven NXP reference design examples for the T1023, LS1043, LS1046 and LS1088 this session will explore the key considerations of each design and show you how to leverage and scale the reference designs for your applications.
查看全文
While many look for hypervisor based solutions when separating multiple operating systems running on multiple cores in the new embedded devices from NXP, an easier solution is often overlooked. This session will describe ARM TrustZone as a technology currently found in the ARM Cortex A family of the devices, but being introduced by ARM in other variants. A few use cases will be presented - these include secure gateway on a Layerscape LS1021 device, and an automotive instrument cluster on an i.MX6 dual core device.
查看全文
Simplify your system design and reduce time to market with integrated mixed-signal microcontrollers with single-die solutions. This lecture will provide an overview of the NXP MagniV portfolio and provide solutions to shrink your applications. Watch Video Presentation
查看全文
This session will provide customers the opportunity to meet with a variety of LPC engineers and marketers to discuss critical topics for today's embedded applications, such as security, connectivity, power consumption, and time-to-market. Attendees will have the opportunity to discuss the latest LPC roadmap, ask technical questions, and provide direct feedback to the LPC leadership team.
查看全文
The Influencers Summit brings some of the smartest and most influential people together to openly share, debate, and learn from one another. The session provides a panel discussion with experts, followed by an opportunity for attendees to participate in roundtable discussions with IoT Security influencers. Topics that will be covered include: What plans are in place for regulating IoT activity? What needs to be done to ensure Security and Privacy concerns do not hinder future developments and deployments of IoT? How do attackers compromise connected devices? What will it take for the technology and business to make it a success? How will we know when we are there?
查看全文
The mil/aero industry is experiencing an increasing demand for COTS DO-254 safety critical solutions. Trends such as the digitization of cockpits, commercial technology complexity, and the use of common avionics subsystems in military and commercial aircraft have solidified the need for DO-254 compliance in military platforms. DO-254 certification was traditionally achieved using costly custom built systems; however, cost-effective COTS modules are now becoming the hardware of choice to reduce the applicant’s risk, time to market, and budget concerns while meeting stringent certification requirements. We will discuss the benefits and concerns of implementing COTS modules for DO-254 certification.
查看全文
The Light Emitting Diode (LED) has revolutionized signaling on control panels and appliances from coffee makers to car dashboards to factory and data center equipment. LEDs give LCD Displays an efficient and more natural backlight, and have upped the ante in dazzling casino and gaming entertainment parlors. Driving and controlling individual LEDs starts with a simple technical question "Constant Voltage or Constant Current?", and is quickly followed by "How many channels do you need?" NXP's LED Controllers are tailored for simple to increasingly complex LED requirements, and take the burden of blinking and fading off your system's microprocessor. Watch Video Presentation
查看全文
The problem of smartphones running out of battery power too soon during the day is well known and in response new fast charging standards have been introduced, ranging from multi-level output ones like USB Power Delivery and Quick Charge to 5V/multi-Amp proprietary Direct Charging protocols. This drives the demand for AC/DC converters with high efficiency over an adjustable 3-20V range, small size, good load step response and very low no-load power. NXP introduces a complete AC/DC fast charging system covering all these requirements, comprising the TEA1936 fly-back controller, the TEA1993/98 synchronous rectifier and the TEA190x family of protocol controllers that communicate with the device to be charged. The TEA190x family supports all mainstream fast charging protocols, is highly configurable and enhances charger safety by an extensive set of hardware integrated protection features.
查看全文