NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
As more and more individuals acquire automobiles and city populations increase, road way congestion worsens year-by-year. Traffic Congestion results in billions of dollars in lost productivity: individuals are confined to hours upon hours of menial vehicle operation in stop-go conditions. Solution: Advances in NXP's ADAS Radar, Vision, and V2X technologies can alleviate congestion and regain lost productivity - 1) reducing personal stress, 2) improving commuter productivity, and 3) reducing traffic accidents. The session will show how controlling driver response variance, (e.g. making acceleration, deceleration, and minimum safe driving distance constant), relieves congestion jamming conditions. The session concludes with a mapping of ADAS DSRC features to NXP devices. Watch Video Presentation
View full article
This beginning hands-on session will walk you through the steps to configure the device and boot U-Boot. Learn how to configure the device reset control word (RCW), flash the device, and debug U-Boot. This session will use the CodeWarrior Development Studio for ARM®v8 ISA to boot the QorIQ LS1021A Reference Design Board (RDB).
View full article
In this section, NXP (SIP) will introduce the key products surround the USB Type-C connectors. The section will covers Power Delivery Controller, Power Delivery PHY, CC logic controller, high speed switch and high speed redriver. We will go over NXP Type-C hardware architecture, differentiation and product advantage.
View full article
This presentation will demonstrate the capabilities of the new i.MX 7 System-on-Chip, a hybrid solution containing a Cortex-A7 processor and a Cortex-M4 processor. Particular attention will be given to the hardware modules and software counterparts allowing both cores to communicate with each other. This hybrid architecture will be highlighted through various potential use cases/product scenarios and a Qt powered application running on top of Linux along with FreeRTOS will be showcased, focusing on asymmetric processing.
View full article
Virtual network functions offer a great deal of flexibility, allowing for dynamic provisioning of network services. Handling network services within a VM and meeting performance requirements can be challenging. It's essential to utilize specialized hardware accelerators to meet the desired performance targets. ODP/DPDK are becoming defacto standard for NFV abstracting the hardware accelerator interfaces from VNF applications. In order to leverage the data plane capability of underlying platform the hardware acceleration can be exposed to the VMs via proprietary interfaces through direct-assignment or standardized interfaces. In this session we discuss how we can leverage the hardware acceleration on QorIQ platforms for developing optimized virtual network functions with DPDK/ODP.
View full article
The QorIQ Communications portfolio has traditionally used Power Architecture® based cores. The latest QorIQ LS series of processors has expanded to use ARM® core technology. There are a lot of software-visible architectural differences between these two types of cores, and system software is dependent on the core architecture. If a system software developer who has experience with Power Architecture based devices transitions to ARM-based processors, the developer must understand the differences between the cores so that the software can be easily migrated from a Power Architecture core to an ARM core. This session compares these two core architectures and sheds light on how software can handle the differences. Watch Video Presentation
View full article
Cars depend on a range of systems that must guarantee safety for their drivers. Linux and Open Source have already entered the infotainment segment, but expanding to ADAS presents new challenges with regards to safety and change control. This session will provide an overview of the internals of the kernel, the safety-critical components, implementation of fault recovery mechanisms and finally how open source software can be used for Autonomous Drive applications. Watch Video Presentation
View full article
NXP offers commercial grade acceleration solutions for common networking applications in non-virtualized and virtualized environments. This session covers NXP’s acceleration solutions landscape on Layerscape and iNIC platforms. Layerscape provides acceleration solutions for Network and Security Applications, Switch Supplementary Applications and OpenFlow Based Applications leveraging LayerScape Accelerated Input Output Processor (LS AIOP).VortiQa-IAAS (Intelligent Application Acceleration Software) offers autonomous SSL processing (SSL termination) and SSL proxy capabilities and VortiQa-IVAS (Intelligent Virtualization Acceleration Software) offers an accelerated infrastructure for NFV (Network Functions Virtualization) to deploy and manage virtual networks and services in VNFs (Virtualized Network Function) on the QorIQ T2 based iNIC. VMM Offload is a NFV solution leveraging LS AIOP.
View full article
Ensuring secure deployment of the billions of end nodes is a key enabler for the Internet of Tomorrow. The Kinetis K8x and Kinetis KL8x families are designed to deliver unsurpassed security for multi-application MCUs with hardware features such as Trust, Cryptographic acceleration, and Anti-Tamper to deliver a scalable, secure platform for embedded developers. This hands-on session will cover the needs of secure embedded applications, performing encrypted firmware updates, utilizing hardware cryptographic accelerators and extending trusted execution to external memories using an on-the-fly AES decryption module. Join this session to learn how your customers can get started creating their next secure node design.
View full article
The NXP supply chain team will present an overview of the new NXP global manufacturing footprint, as well as integrated strategies for supply assurance and crisis management. An overview of current supply chain systems integration activities will be discussed as well as customer order management strategies moving forward. A special focus will be placed on highlighting changes that will affect NXP customers. Watch Video Presentation
View full article
High speed internet always and everywhere is the challenge we are facing. Small cells provide the solution to fill the coverage gaps of the regular basestation infrastructure. This lecture shows the NXP high performance RF solutions to cover both the transmit and receive side of the small cells.
View full article
This session explain how to achieve a higher level of security with NXP's latest NFC controller solution with customizable firmware, the PN7462, using a Secure Access Module (SAM) for applications like corporate access. The session follows the NFC access control hands-on workshop with a particular focus on security. In this session the PN7462 development kit will be used to demonstrate how high security using MIFARE DESFire EV1 and a SAM can be achieved.
View full article
Countless devices are joining the Internet of Things (IoT) daily. It is a key requirement that the device architecture of the device itself is secure; above and beyond the mandatory connection privacy. Embedded devices also require a device security approach that can follow future security trends, changes, and threats throughout their entire product lifecycle. This session looks at reported cases of device vulnerability in the industry, available technology, and best practices for designing secure connected products. Based and built on the Digi ConnectCore for i.MX6UL connected SOM platform, and without the traditional burden of effort related to design and implementation.
View full article
New entrepreneurs and innovators today can quickly prototype, thanks to the new Maker movement. This seemingly endless world of possibilities, however, hits a strong limitation when it comes to manufacturing a product in mass production, due to a missing step, or link, between making a proof of concept and manufacturing it. This speech, will show how SECO picked up on the gap between Makers and Industry, by fusing its embedded expertise with the newly acquired Maker Movement experience, through its community movement and board: UDOO.
View full article
This session will provide a detailed introduction to NXP's HomeKit Software Development Kit (SDK) architecture, APIs and code adaptors. Through hands-on examples, you will learn accessory profile configurations, how to integrate with accessory application software, and how to build and debug a demo accessory (Restricted to verified MFi licensees only).
View full article
AC/DC converters need to provide a defined and safe supply voltage from AC mains, varying from 90 to 264 V AC. Key requirements are efficiency, no-load power consumption and size. A new requirement for wall chargers is communication to the mobile, enabling faster charging by changing voltage or current. Most common AC/DC topologies are flyback and resonant. A flyback converter features lowest cost, but magnetics size becomes larger at higher output power. In that case, resonant converters are preferred, although efficiency is lower at low loads. NXP has invented a resonant concept that overcomes this issue. The presentation will introduce the mentioned AC/DC technologies and NXP’s product advantages.
View full article
The first step to creating a smart sensor algorithm is collecting sensor data for analyses. This session will present a series of sensor data logging options which allow engineers to create dataloggers quickly using Kinetis SDK framework by including IS-SDK without having to concerning themselves with any mudance sensor integration efforts. Watch Video Presentation
View full article
Aimed to be a hands-on the exercise would consist in using a vision processor to run CNN on various pictures to recognize traffic signals (Stop, Turn, Yield, etc). First we will cover basic concepts on machine learning for the algorithms to be used. After the class part is over, we will use a vision processor to run CNN to recognize between traffic signs and no traffic signs.
View full article
A look at new types of low- or battery-powered and space-constrained applications made possible be the latest innovations in communications processors, including portable storage, IoT Gateways and embedded control.
View full article
This beginning hands-on session will walk you through the steps to configure the target and tools to debug applications running on Linux. Learn about agent based debug and tools to view the Linux OS state. This session will use the CodeWarrior Development Studio for ARM®v8 ISA with a QorIQ LS series Reference Design Board (RDB).
View full article