NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
This hands-on workshop will help you get started with our latest MAC57D5xx processor for instrument cluster and human machine interfaces together with the recent release of MQX. Practical use cases will be demonstrated and exercised during this hands-on workshop session.
View full article
Many customers struggle getting their first GUI design running, and often this results in schedule and budget problems. This class covers the issues and SOLUTIONS required to get a Graphical User interface up and running. We provide solutions to standard embedded communication requirements like Ethernet, USB, Wi-Fi, and Serial. We present a Case Study of a new product using a touch screen GUI, LEDs and audio to communicate the fluid level and temperature of a beverage container back to the user. We cover the pros and cons of developing your own software or of using proven off-the-shelf solutions based on standard building blocks. We also address the buy vs. make hardware decision and look at time to market and risk factors. The class ends with a demonstration of the solution implemented with an off-the-shelf NXP LPC microcontroller based hardware module and simple custom expansion board.
View full article
Introduction to QN9020 development board and SDK and design with QN9020 for wearables and IoT devices plus integration NXP BLE features into iOS or Android app.
View full article
Simplify your system design and reduce time to market with integrated mixed-signal microcontrollers with single-die solutions. This lecture will provide an overview of the NXP MagniV portfolio and provide solutions to shrink your applications. Watch Video Presentation
View full article
This session will provide an overview of NXP automotive sensors for airbags, TPMS, ABS, engine management and other safety and comfort applications.  Watch Video Presentation
View full article
Designing solid state RF solutions to deliver controllable, high efficiency energy for consumer cooking appliances requires designers to carefully consider size, cost, and performance objectives. This session will cover NXP's approach to a scalable, modular platform for delivering controllable RF energy for integration into cooking appliances. Watch Video Presentation
View full article
Introducing a new Brushed DC motor driver product family designed for automotive engine control applications. It will be the first motor driver fully certified to ISO26262 to support ASIL level D system qualification and features a patented thermal management scheme to ensure high, efficient operation. The key aspects of thermal power dissipation during heavy load conditions will be reviewed. The session will also include a demonstration with the new brushed dc motor driver and SPI GEN software, showing its integrated protection features. The participants will be able to see how current averaging will maintain higher torque during over-load and all the safety features that can be reported over the SPI.
View full article
The QorIQ Communications portfolio has traditionally used Power Architecture® based cores. The latest QorIQ LS series of processors has expanded to use ARM® core technology. There are a lot of software-visible architectural differences between these two types of cores, and system software is dependent on the core architecture. If a system software developer who has experience with Power Architecture based devices transitions to ARM-based processors, the developer must understand the differences between the cores so that the software can be easily migrated from a Power Architecture core to an ARM core. This session compares these two core architectures and sheds light on how software can handle the differences. Watch Video Presentation
View full article
This session will provide an introduction to developing Made For iPod (MFi) accessories including audio, non-audio, CarPlay, AirPlay and HomeKit applications based on NXP microcontrollers (MCUs), microprocessors (MPUs), HomeKit Software Development Kit (SDK), MFi SDK, and software from NXP Professional Services.
View full article
Experience the power of market leading real time operating system, FreeRTOS and Kinetis MCUs. Learn with experts about the FreeRTOS and how to enable FreeRTOS on Kinetis MCU's: Creating a Kinetis SDK project with FreeRTOS and Kinetis Design Studio, configure it for best code size and performance, debug it with Kernel Awareness in Eclipse and how to get detailed application and systems performance data using FreeRTOS+Trace performance analysis tools.
View full article
This session will provide customers the opportunity to meet with a variety of LPC engineers and marketers to discuss critical topics for today's embedded applications, such as security, connectivity, power consumption, and time-to-market. Attendees will have the opportunity to discuss the latest LPC roadmap, ask technical questions, and provide direct feedback to the LPC leadership team.
View full article
Learn how to improve your design cycle time and system efficiency with the new Kinetis Motor Suite (KMS) software solution. Built on the high performance Kinetis V Series MCUs, KMS makes motor control simple for any experience level. In this hands-on class we will take you from initially turning you own motor to building your first custom application using KMS. Bring your own PMSM motor and learn how to get it spinning and tuned in minutes.
View full article
This session will provide a demonstration led by the instructor that showcases how you can develop end products using the application solution kit (ASK) for QorIQ LS1043A processors. Watch Video Presentation
View full article
Healthcare is ripe for disruption. In this class we will outline how NXP IoT products enable a variety of healthcare solutions that will lower patient costs and improve patient outcomes. Watch Video Presentation
View full article
This session will discuss which analysis tool to use and when. Through customer success stories of using the CodeWarrior Analysis Tools, you will learn how to overcome business critical software issues, improve application performance and meet criteria for quality requirements. Watch Video Presentation
View full article
This presentation will look at the lessons learned from vehicle hacks and introduce a whole vehicle multi-layered approach to automotive security. In 2015, automotive security was rarely far from the headlines of technical and public media, with a number of very public hacks of some major vehicle brands. The result was a renewed focus on vehicle security. There will be an introduction to the NXP portfolio of automotive products from microcontrollers, secure transceivers and secure elements and how they all fit together to offer a complete security solution for connected vehicles today and tomorrow.
View full article
NXP offers commercial grade acceleration solutions for common networking applications in non-virtualized and virtualized environments. This session covers NXP’s acceleration solutions landscape on Layerscape and iNIC platforms. Layerscape provides acceleration solutions for Network and Security Applications, Switch Supplementary Applications and OpenFlow Based Applications leveraging LayerScape Accelerated Input Output Processor (LS AIOP).VortiQa-IAAS (Intelligent Application Acceleration Software) offers autonomous SSL processing (SSL termination) and SSL proxy capabilities and VortiQa-IVAS (Intelligent Virtualization Acceleration Software) offers an accelerated infrastructure for NFV (Network Functions Virtualization) to deploy and manage virtual networks and services in VNFs (Virtualized Network Function) on the QorIQ T2 based iNIC. VMM Offload is a NFV solution leveraging LS AIOP.
View full article
Learn the benefits and advantages of our MAC57D5xx product family, targeted for instrument cluster and industrial human machine interface applications.
View full article
Providing power for the latest processors used in ADAS systems combines best practices from both the automotive and networking disciplines. Linear Technology’s deep knowledge in both fields and years of supporting applications for automotive and networking systems, including new standards such Power Over Data Line (PoDL) will ensure a robust power supply network for your applications. In this session Dave Dwelley, Office the CTO at Linear Technology, will discuss a roadmap to success as the data center on wheels becomes a reality.
View full article
Recent trends are moving toward a Linux user space as an environment for packet processing. Hardware vendors have provided their own API in the user space for accessing data plane functions like sending and receiving packets, classification, scheduling, and acceleration. As the market matures, a shift toward a common API is allowing a degree of portability across hardware platforms. For DPDK or ODP, efforts are in place to create a platform independent and vendor-neutral standard API for optimized packet processing and traditional networking services. This session will provide a comparative analysis and evolution of both of these standards. We'll discuss how NXP is working to provide support for these common API without sacrificing performance or leveraging specific acceleration advantages of the NXP data plane architectures.
View full article