NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
This presentation will cover the Hardware Security Module (HSM) and how to use the software kits NXP offers, the HSM Security Firmware and HSM Software Development Kit. We will also cover other security features of the device offered by modules like PASS or TDM and their configuration. Watch Video Presentation
View full article
NXP’s latest generation of passive UHF RFID, called UCODE® DNA, can be used in Automatic Vehicle Identification (AVI) systems that make it easier to identify – and collect from – drivers of vehicles that aren’t properly registered. In an AVI system for vehicle registration, readers can be installed above, below, or to the side of the road. They can also be embedded in a handheld device, for use by government personnel. The tag, attached to the vehicle, uses the energy produced by the reader’s RF field, so there’s no need for a battery and the tag has a very long lifespan. Cryptography-based security minimizes errors and practically eliminates fraud. Vehicle owners (and fee collectors) can be confident that the right person is being billed, since readings are both highly accurate and highly secure.
View full article
Combining traditional MCU features with high voltage analog components in a single chip saves you system cost. An integral solution that improves quality and reduces footprint. This is an overview of the S12 MagniV MCU family for closure solutions such as window lift, sunroof, and sliding doors.
View full article
NFC enables new interfaces and use cases in the Automotive domain, such as car access and start, vehicle personalization, quick and easy connectivity and secure payment. In this session we will cover NFC working principles, NFC enabled use cases, like smartphone vehicle access and secure simple pairing, and the challenges for NFC in Automotive applications. A demo will illustrate the working principles of NFC based car access. Watch Video Presentation
View full article
There is an increasing number of high/ultra high speed drives required by the industry. The theory offers the rules how to drive fast motors, however not all them are easily applicable in the real word. The significant issue is that the rules requires a pretty powerful device to be enough fast to control fast motors. The presentation offers the comparison of the theory with the experiences out of the customer project targeting the high speed motors controlled by a less powerful devices, where the less powerful controller is a pretty challenge within the overall task.
View full article
NXP supplies cutting edge hardware and software tools for ADAS development. The software algorithm developer will encounter a heterogeneous tool environment that may prove to be challenging. In this session, we will walk through NXP's enablement offerings for ADAS algorithm development and explain how to use these tools to implement a sensor input data path for Blue Box. This session will review the heterogeneous tool landscape, including AUTOSAR drivers, Inter-Core Communication and PCIe on S32V, as well as LS2 Root Complex Driver and LS2 Linux data management of critical safety data. Attendees will leave with a clear picture of how to leverage NXP's tools in ADAS development.
View full article
As more and more individuals acquire automobiles and city populations increase, road way congestion worsens year-by-year. Traffic Congestion results in billions of dollars in lost productivity: individuals are confined to hours upon hours of menial vehicle operation in stop-go conditions. Solution: Advances in NXP's ADAS Radar, Vision, and V2X technologies can alleviate congestion and regain lost productivity - 1) reducing personal stress, 2) improving commuter productivity, and 3) reducing traffic accidents. The session will show how controlling driver response variance, (e.g. making acceleration, deceleration, and minimum safe driving distance constant), relieves congestion jamming conditions. The session concludes with a mapping of ADAS DSRC features to NXP devices. Watch Video Presentation
View full article
This session will cover the different vision processing capabilities of the S32V234 automotive vision processor with a focus on the Image Sensor Processor (ISP). The presentation will demonstrate how the cost of a vision system can be cut down by using the ISP to accept raw camera input data and to process it using algorithms like debayering, white balancing, format conversion, HDR and de-noising. The aim of the session is to give an introduction to camera processing, to present the architecture of the ISP and to demonstrate how it can be programmed using a visual tool developed by NXP.
View full article
The session will provide an overview of the most recent developments to support Radar systems in the frequency range from 76 GHz up to 81 GHz. High level block diagrams and key specifications of NXP multi-channel transceivers will be presented. It will also be discussed how the NXP transceiver solutions can help to enable modern low power consumption sensors with robustness against frequency interference, small size, and high-performance due to scalability. In combination with NXP Radar micro-processors and mircro-controllers typical Radar system architectures will be introduced. Especially for the development of small and compact cocoon, nano radar sensors an example is presented which shows the combinations of NXP Radar tranceivers, NXP Radar processors and NXP power supply solutions. The presentation will also give an outlook to technology trends and future upcoming NXP Radar solutions.
View full article
Building on top of 11 years of usage within data centers, Xen Hypervisor is uniquely placed to support a new range of use cases for embedded solutions. In particular, its isolation and security features, flexible virtualization modes and architecture, driver disaggregation, and strong ARM support make it a perfect fit for embedded applications. Artem Mygaiev, GlobalLogic’s Embedded Practice Head, will explore the virtualization nuances and challenges of using Xen Hypervisor for embedded applications through the demonstration of his own company’s journey in developing a platform that leverages Xen for virtual network equipment, IoT, automotive, and other embedded use cases.
View full article
Cars depend on a range of systems that must guarantee safety for their drivers. Linux and Open Source have already entered the infotainment segment, but expanding to ADAS presents new challenges with regards to safety and change control. This session will provide an overview of the internals of the kernel, the safety-critical components, implementation of fault recovery mechanisms and finally how open source software can be used for Autonomous Drive applications. Watch Video Presentation
View full article
With new CAN FD protocol, CAN applications need to support both classical CAN and CAN FD frames. Especially in transition period, customers are looking for a solution in which classical CAN frames are mixed with CAN FD frames. NXP developed a brand new CAN transceiver feature "CAN FD Shield", which enables the use of CAN controllers in mixed CAN / CAN FD architectures. Watch Video Presentation
View full article
This session is a high level introduction to the problems to tackle for automated driving and sensor fusion applications. It describes NXP’s BlueBox solution, the first motion-planning system to address the stringent safety, power and processing performance requirements of the world’s top automakers. This session will also review BlueBox performance capabilities required to analyze driving environments, assess risk factors and then direct the car’s behavior. Watch Video Presentation
View full article
Vehicles need to accurately grasp the world around them - just like the human driver - in order to drive autonomously. Automotive technology aims to fit vehicles with capabilities even beyond the senses of the human driver, allowing to make the most intelligent decisions in real time. The information that vehicle sensors collect must not only be real time and accurate but also be secure against hacking attacks so that we can trust them with our lives. Reliable ADAS and appropriate security measures are a key ingredient in self-driving cars. Vehicle-to-X technology, extends the visibility beyond the sight of drivers to "see" around corners and through obstacles. External sensor information and internal data from the car networks are vital to help to eliminate the 1.3 million road accidents happening on global roads each year.
View full article
Get up and running in minutes with the NXP S32K platform using the S32 SDK and S32 Design Studio. This hands-on session will introduce the full flexibility and capability of the S32 SDK package, outlining the excellent out-of-the-box experience, ease of use and shorter time to market. Attendants will learn how to use it in correlation with S32 Design Studio IDE to quickly create suitable applications for general-purpose use-cases, running through all the development steps (installation, software configuration & RTOS integration, inserting application code and target debug).
View full article
This session reviews the updates to the existing Linux Software Development Kit (SDK) which allows for the enablement of the Blue Box software feature set. Custom layers, simplified deployment, support for multiple SoCs in one set-up, a graphical desktop, package management, self-hosting support and other additions will be described in technical detail. Options to further enhance the configuration will also be discussed. Software engineers interested in Yocto customizations should not miss this session.
View full article
The need to ensure electrical power availability is increasing. Batteries are spreading into automotive, electrical storage systems and uninterruptible power supplies. This session will present the benefits of NXP Battery Management Solutions for multiple battery architectures. Watch Video Presentation
View full article
V2X technology has the potential to drastically reduce road accidents and improve the traffic flow by fusing in-car sensor data with data obtained from other road users and from the surrounding infrastructure - visibly or unvisbily and far beyond the driver's line of sight. Vehicle to cloud data communication provides a pathway for anonymous data collection and dissemination. When the true potential for V2X is realized and it becomes a true part of the vehicle safety system it is vital that the authenticity and security of data are guaranteed. In addition, the vehicle control units that coordinate active stability systems must be protected against external influences that might subvert the mechanisms design. This presentation will explore the various security countermeasures needed to make V2X a safe and secure technology for the future. Watch Video Presentation
View full article
Automotive headlamp technology is rapidly changing. LEDs are used increasingly in automotive lighting applications to enable creative design elements, improve system efficiency and enable advanced driver assistance system (ADAS) features. Car makers and lighting tier 1s are looking for flexible and scalable solutions that can quickly enable ADAS functionality across multiple car platforms to increase re-use and reduce development time and cost. NXP has released a state of the art Multichannel LED driver portfolio to address these emerging advanced lighting applications. The LED drivers provide all the necessary functionality to ensure a compact, low-cost and flexible design for advanced LED headlights. In this session learn how our LED drivers address the key trends and current and future requirements for advanced LED headlights. See the demo for your self! Watch Video Presentation
View full article
During this course we will review how to use the new analog Freedom board FRDM-12XSF available for 12V eXtreme Switch devices thanks to the analog Processor Expert software and Kinetis Design Studio component. This training will cover full system enablement from hardware (MCU + analog), software (MCU agnostic) perspectives and demonstrate how to quickly drive different type of loads (resistive, inductive and capacitive). Thanks to its processor eXpert component, the interaction between MCU, sensor and our device will be facilitate, this training will cover different exercise to make the trainee fully enabled.
View full article