X.509 Certification on the Mifare DESFire EV2 Key Fob

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

X.509 Certification on the Mifare DESFire EV2 Key Fob

400 Views
Konsti
Contributor I

Hello,

we have KeyFobs in use in our company for time recording and physical access control. And now we want to use them for MFA as well. So that the employees authenticate themselves on the PC (Windows 10) and applications. We already have a PKI infrastructure in place.

My question: Is it possible to put an X.509 on the following Key Fob?

Time and attendance
ISO14443A-MIFARE DESFire EV2 ' EEPROM 8 kB ' UID Length 56 Bits ' UID HEX 043828xxxxxx

Access
EM4x02 ' UID Length 40 Bits ' UID HEX 011149Axxx

 

If it works; Is there a standard for this or do you have to access special manufacturing solutions?

 

Tanks

 

0 Kudos
0 Replies