PN5180 Datasheet minor fix suggestion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 Datasheet minor fix suggestion

450 Views
ryan4volts
Contributor I
Reading through the PN5180A0xx_C3_C4 Rev 3.7 (3/2/2021) in table 51 Page 49 to 50 the "Random UID enable field is duplicated to both EEPROM addresses 0x51 and 0x58. However the FELICIA_POLLING_RESPONSE is set to address 0x46 of size 18 bytes. Thus it would take up 0x46 -> 0x57 (Inclusive). So I believe the 0x51 Random UID enable address is incorrect. Despite in the description for both the 0x51 and 0x58 referring only to the 0x51 address. So this is a little confusing to follow.
0 Kudos
1 Reply

443 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your information. We will forward it to the related team.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos