PN512 NXP Expansion with Type B Tags

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN512 NXP Expansion with Type B Tags

1,640件の閲覧回数
bassembadawi
Contributor I

Dear community,

is it possible to read out NDEF messages from ISO 14443B Tags with the example software from Expansion Board for the Raspberry Pi?

I´m using a passiv sensor Tag (TI Tida00217) with a RF430CL330HCPW Transponder on it. If it is not possible with the example software how I can use the Type B functionality from the pn 512.

Best regards,

Bassem

タグ(1)
3 返答(返信)

1,292件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Bassem,

I have a script for PN512EV to reader the type B card, you may use it as a reference.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,292件の閲覧回数
manojrohitvempa
Contributor II

Hello Kan_Li,

Do you think the API's in 'NFC Reader Library' could be used to read Type 4B tags?

0 件の賞賛
返信

1,292件の閲覧回数
bassembadawi
Contributor I

Thanks Kan_Li

that really helps a lot!

0 件の賞賛
返信