NXP Taginfo app just doesn't read tags on iphone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Taginfo app just doesn't read tags on iphone

5,966 Views
daveb1
Contributor II

We're just starting out and are trying to read tags with phones.

We downloaded and ran Taginfo on Android phones and it just works (after turning on NFC in settings)

Downloading and running the Taginfo app on 3 different iPhones - and nothing happens. It launches, wait for a tag, but nothing we do can get any read to happen.

Is there something we're missing (like turning on NFC on Android)?

10 Replies

4,512 Views
luca_securo
Contributor III

Hi to all,

   I have any problems with Iphone too.

In my case, the Iphone doesn't read the NDEF memory of NT3h2111 Ntag I2c Plus.

I changed the Ntag with NT3H2211 (or 1211) and Iphone can read the tag.

The antenna is the same and the app is NFC TagInfo.

The difference is the NDEF memory capacity (1KByte against 2KByte).

Is it possible that Iphone can't read 1KByte NDEF memory?

Any suggestion?

Android have no problems.

Thank you!

Have a nice day!

Luca

0 Kudos
Reply

4,512 Views
driesmoors
NXP Employee
NXP Employee

Hi Luca,

Your iPhone should have no problems reading 1KByte of data or more - I've already tried it with 8KByte of data without any issue.

Did you already check with another APP or an Android phone whether the contents of the tag contains a proper NDEF message?


Can you share the raw tag contents? For example, using an Android phone running the NXP APP Tag Info.

Best,
Dries.

0 Kudos
Reply

4,512 Views
luca_securo
Contributor III

Hi Dries, thanks for reply.

I tried to reset the tag with NTag I2C Demo app for android.

Now it works, you are right!

However It's strange becouse Android never had reading problems.

Thanks!

Have a nice day!

Luca

4,512 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Dave Bush,

I would also recommend to verify that the format of the card is NDEF and that is have stored an NDEF Message, IOS allows only to read NDEF messages from NDEF formatted cards,  some cards like smartcards used in transport or other applications cannot be read with Iphone,  you do not have to activate the NFC, once the application is running the NFC reader of the phone starts polling, this is a difference from android that you can turn on of off the NFC module at any time. 

hope this helps your question.

BR

Jonathan

4,512 Views
daveb1
Contributor II

Ahhh. Thank you.
On Android you get the "ID" of the tag, so we've been testing with empty tags.
From this it looks like we have to put data in the tag.
We''ll try that and see how it goes.

0 Kudos
Reply

4,512 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

yes and please check the card is formatted as NDEF.

BR

Jonathan

0 Kudos
Reply

4,512 Views
driesmoors
NXP Employee
NXP Employee

Hi,

Sorry to hear this. My personal experience with iPhones is actually very good when it comes to NFC. Which iPhone model did you try? Did you see the iOS popup informing you can now scan a tag?

   

Best,
Dries.

0 Kudos
Reply

4,512 Views
daveb1
Contributor II

No nothing like that. The app just launched and said ready to Scan - and that was it,

0 Kudos
Reply

4,512 Views
driesmoors
NXP Employee
NXP Employee

Ok. Here are my screenshots when I use the APP:

After launching "NFC TagInfo", pastedImage_1.png

I just click on "Scan & Launch" pastedImage_2.png

Then the popup comes, pastedImage_3.png

and I can tap with my phone the tag, which is instantly read.

Can you share your screenshots? 

0 Kudos
Reply

4,511 Views
daveb1
Contributor II

Thanks - our iPhone isn't in until next week !

0 Kudos
Reply