Explore-NFC compatibility with ISO-14443 Type 4B tags

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Explore-NFC compatibility with ISO-14443 Type 4B tags

1,053 Views
manojrohitvempa
Contributor II

Hello guys,

I have downloaded the NFC Reader Library from http://www.nxp.com/pages/:NFC-READER-LIBRARY. I downloaded the previous Version "NFC Reader Library for Linux" version 4.040.05.011646". Because the latest library for Linux is not compatible with explore-NFC board.

I was able to detect Type 4B tag as I was able to obtain the UID. But I am not able to obtain the Ndef message.

When I run the 'NfcrdlibEx3_NFCForum' I was able to detect the NDEF message for Mifare Cards. But not for Type 4B tags. Is there any example I am missing which can read NDEF Messages with explore-nfc.

Thank you in advance. 

0 Kudos
0 Replies