MCRSP_PMSM_V1.2.0 with LPC15xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCRSP_PMSM_V1.2.0 with LPC15xx

ソリューションへジャンプ
2,597件の閲覧回数
peterkostadinov
Contributor III

Hello,

Is it possible to use MCRSP_PMSM_V1.2.0 with LPC15xx?

Best Regards,

Peter

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,495件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Peter,

You can refer to the Field Oriented Control of PMSM motor using LPC15xx. Here you will find the following:

This Zip file contains following items.
1) FOC Application Note
2) FOC PMSM firmware source V1.1 based on IAR toolchain
3) LPC1500 motor Control GUI v1.1
4) You can also use terminal program to send command to firmware.Change GUI_Interface=1 to GUI_Interface=0
to use firmware with terminal

Note: This firmware contains FOC control of PMSM motor in QEI sensored mode

Best Regards,

Sabina

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,495件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

This release has been on and supports the following development platforms:

pastedImage_1.png

Unfortunately, this does not include the LPC.

Best Regards,

Sabina

0 件の賞賛
返信
2,495件の閲覧回数
peterkostadinov
Contributor III

Hi Sabina,

Thank you for the replay.

If there is some example project with LPC15xx and FOC (without MCRSP_PMSM)?

Best Regards,

Peter

0 件の賞賛
返信
2,496件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Peter,

You can refer to the Field Oriented Control of PMSM motor using LPC15xx. Here you will find the following:

This Zip file contains following items.
1) FOC Application Note
2) FOC PMSM firmware source V1.1 based on IAR toolchain
3) LPC1500 motor Control GUI v1.1
4) You can also use terminal program to send command to firmware.Change GUI_Interface=1 to GUI_Interface=0
to use firmware with terminal

Note: This firmware contains FOC control of PMSM motor in QEI sensored mode

Best Regards,

Sabina

0 件の賞賛
返信
2,495件の閲覧回数
peterkostadinov
Contributor III

Hi Sabina,

Thank you very much!

Best Regards,

Peter

0 件の賞賛
返信