MPC5744P DSPI example,A vital problem occurs.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P DSPI example,A vital problem occurs.

830 Views
秦祥林秦
Contributor I

When I use the MPC5744P DSPI examples, I find a problem.DSPI initialization process in the skip DISAB_IRQ (), directly into the DSPI_init.However, when the shield DSPI_init, the program has returned to normal.The initial value of the DSPI is not passed, and the default value becomes all 0.

0 Kudos
Reply
1 Reply

682 Views
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

This community is about issues encountered with the Model-Based Design Toolboxes. As far as i can see from your attachment you are using stand-alone examples for MPC5744P.

Since you are not using Matlab/Simulink to generate the code automatically for DSPI on MPC5744, my suggestion to you is to ask this on a different community: MPC5xxx or the place you have took the examples from.

Thank you!

Daniel 

0 Kudos
Reply