MBDT - DS : No rule to make target (.ld)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT - DS : No rule to make target (.ld)

1,764 Views
Chandra13
Contributor I

Hello,

I generated the c code for gpio_s32k148.mdl from the NXP_MBDToolbox_S32K1xx in Simulink and would like to import them (used the ProjectInfo.xml to import the project) to the Design Studio and be able to build and flash the elf.

The compiler in DS throws an error, "No rule to make target" for a ld file, but the generated code has the necessary linker files. I am not sure why the DS is failing to locate it. (Refer Error1)

To correct the Error1, I had copied the "S32K14x.ld" file to the workspace location and I get an error that does not give any information. (Refer Error2)

Project Details,

  1. S32K148-Q176
  2. Design Studio 3.4
  3. Matlab R2022b
  4. NXP_MBDToolbox_S32K1xx 4.3.0

 

0 Kudos
Reply
0 Replies