square waves with different frequencies on FTM2 of KEA-128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

square waves with different frequencies on FTM2 of KEA-128

855 次查看
vignesh_vb_7
Contributor IV

Hi,

I want to generate square waves of multiple frequencies by using FTM2 of KEA-128.For this I have to update the values of FTM2_CnV,FTM2_MOD and FTM2_CNTIN.I am not able to update these values properly.

volatile unsigned long duty =0x00000080;

void Clk_Init()

{

ICS_C1|=ICS_C1_IRCLKEN_MASK;  /* Enable the internal reference clock*/

ICS_C3= 0x90; /* Reference clock frequency = 31.25 KHz*/

while(!(ICS_S & ICS_S_LOCK_MASK));   /* Wait for PLL lock, now running at 40 MHz (1280 * 31.25Khz) */

    ICS_C2|=ICS_C2_BDIV(1)  ;  /*BDIV=2, Bus clock = 20 MHz*/

ICS_S |= ICS_S_LOCK_MASK ;  /* Clear Loss of lock sticky bit */

}

void FTM_Init()

{

SIM_SCGC |= SIM_SCGC_FTM2_MASK; /* Enable Clock for FTM2 */

SIM_PINSEL1 |= 0x00000008;      //selecting pin F1

       

  //      FTM2_MODE |= FTM_MODE_FTMEN_MASK; /* FTM2 enabled */

       

        /* Mask the output channels for safe state */

        FTM2_OUTMASK |= FTM_OUTMASK_CH1OM_MASK; /* FTM2 ch1 output mask */

       

        /* Set Modulo */

        FTM2_MOD = 0xFFFFFFFF;

         ; /* 0xFF(255) + 1 = 256 counts */

       /* Channel 1 : Edge-alined PWM */

        FTM2_C1SC |= FTM_CnSC_MSB_MASK;  /* Channel as Edge-aligned PWM mode */

        FTM2_C1SC |= FTM_CnSC_ELSB_MASK; /* High-true pulses */

        /* Set period value */

        FTM2_C1V = duty;

       

       

       

       

       

        /* write any value to CNT in order to reset FTM Counter and update the channels output according to new configuration */

        FTM2_CNT = 0x00000001;

       

        /* Clock setting */

        FTM2_SC |= FTM_SC_PS(4); /* Select Prescaler in this case 1.  20Mhz /16 =1.25Mhz. */

        /* (1/1.25Mhz) = 0.8 microsec */ /*Counter increase by one every 0.8 microsec */

        FTM2_SC |= FTM_SC_CLKS(1); /*FTM2 use system clock*/

       

        FTM2_SYNCONF |= FTM_SYNCONF_SYNCMODE_MASK; /* for PWM duty updating sync by SWSYNC */

        FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK; /* for PWM duty updating sync by SWSYNC */

        FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK; /* for PWM duty updating sync by SWSYNC */ // selects software trigger as PWM synchronization

        /* Unmask the output channels */

        FTM2_OUTMASK &= ~FTM_OUTMASK_CH1OM_MASK;

       

}

void main(void)

{

 

Clk_Init();     /* Configure clocks to run at 20 Mhz */

FTM_Init();    /* Initialize the FTM module */

        FTM2_PWMLOAD |= FTM_PWMLOAD_LDOK_MASK; /* Loading updated values is enabled */

       

for(;;) {

    UINT8 i;

   

          FTM2_COMBINE |= FTM_COMBINE_SYNCEN1_MASK;       /* PWM synchronization between pair of channels */

              FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

          FTM2_C1V = 0x952;

          FTM2_MOD = 0x12A4;  

          FTM2_CNTIN = 0x00000001;                                                                                                                                             //HAP

          FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;// generate software trigger to change the duty value

  

      FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

      FTM2_C1V = 0x952;

      FTM2_MOD = 0x12A4;

      FTM2_CNTIN = 0x00000001;                                                                                                                                                        //py

      FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;// generate software trigger to change the duty value 

   

   

  FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

  FTM2_C1V = 0x86C;

  FTM2_MOD = 0x109C;                                                                                                                                                                          //birth

  FTM2_CNTIN = 0x00000001;

   FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;// generate software trigger to change the duty value 

  FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

FTM2_C1V = 0x952;                                                                                                                                                                                        //Day

FTM2_MOD = 0x12A4;

FTM2_CNTIN = 0x00000001;

FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;// generate software trigger to change the duty value   

   

 

FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

FTM2_C1V = 0x6FF; 

FTM2_MOD = 0xDFE; 

FTM2_CNTIN = 0x00000001;                                                                                                                                                                                   //TO

FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;// generate software trigger to change the duty value  

   

FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

FTM2_C1V = 0x766; 

FTM2_MOD = 0xECC;                                                                                                                                                                                             //YOU

FTM2_CNTIN = 0x00000001;                                                                                               

FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;// generate software trigger to change the duty value 

       

}

}

0 项奖励
回复
1 回复

690 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Vignesh,

I suggest you enable FTM overflow interrupt, in the ISR of FTM overfolw, you can update the FTM2_C1V, FTM2_MOD, FTM2_CNTIN. If you do want to update the registers in for() loop, I think you can set a flag in the ISR of FTM overflow, in the for() loop, poll the flag, if the flag is set, update the registers, and clear the flag so that ISR can set it again.

There are several methods to update the registers, I suggest you read the an5142 from the website:

http://tinyurl.com/ppwqetz

The application note include the code to update the register with software updating or with LOAD updating.

It is not appropriate to update the register in main for() loop as you have done, because it is too frequent to update the FTM register in the for() loop.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复