Where can I find a BSP for the TWR-MCF51CN?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find a BSP for the TWR-MCF51CN?

Jump to solution
652 Views
TBRTech
Contributor I

I've searched all over, except in the right place.

0 Kudos
1 Solution
550 Views
anthony_huereca
NXP Employee
NXP Employee

Just to add a little bit to Zhang's explanation, several legacy BSPs were retired in MQX 4.0.0 in order to focus on newer processors and features. These boards are listed in the MQX release notes under Version 4.0.0 changes, and as pointed out above, MQX 3.8.1 is still available for free download if you need access to these BSPs.

The following board support packages were removed from the release and will be supported only as a part of MQX 3.8.1 version maintenance.

o TWR-MCF51AG, TWR-MCF51CN, TWR-MCF51JE, TWR-MCF51MM, TWR-MCF51QM, DEMOEM, DEMOAC, EVB51JM128, M5208EVB, M52223EVB, M52233DEMO, M52235EVB, M52277EVB, M53015EVB, M5329EVB, M54455EVB and MPC8308RDB

-Anthony

View solution in original post

0 Kudos
7 Replies
550 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

on my side, my mqx4.0.2 doesn't include 51cn bsp, but mqx3.8.1 includes it. here is its download link:

Freescale MQX™ Software Solutions Product Summary Page

0 Kudos
551 Views
anthony_huereca
NXP Employee
NXP Employee

Just to add a little bit to Zhang's explanation, several legacy BSPs were retired in MQX 4.0.0 in order to focus on newer processors and features. These boards are listed in the MQX release notes under Version 4.0.0 changes, and as pointed out above, MQX 3.8.1 is still available for free download if you need access to these BSPs.

The following board support packages were removed from the release and will be supported only as a part of MQX 3.8.1 version maintenance.

o TWR-MCF51AG, TWR-MCF51CN, TWR-MCF51JE, TWR-MCF51MM, TWR-MCF51QM, DEMOEM, DEMOAC, EVB51JM128, M5208EVB, M52223EVB, M52233DEMO, M52235EVB, M52277EVB, M53015EVB, M5329EVB, M54455EVB and MPC8308RDB

-Anthony

0 Kudos
550 Views
TBRTech
Contributor I

btw, I did a live chat trying to get help.  He suggested getting FreeRTOS instead!  Not that it's really free, since you have to pay for the documentation about how to use it.

0 Kudos
550 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

can you please specify why need to pay for the document?

0 Kudos
550 Views
TBRTech
Contributor I

I didn't see where they had documentation available except in their store where they want $30 for a PDF of the reference manual (here's the link)

FreeRTOS software, hardware and education shop

0 Kudos
550 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

i never use freeRTOS but i just perform search in google i find some other resource:

http://www.freertos.org/RTOS.html

did you ever check them.

0 Kudos
550 Views
TBRTech
Contributor I

Thanks!  Now all I have to do is figure out how to get at it.

0 Kudos