NullPointerException when opening user_config.h - what have I misinstalled?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NullPointerException when opening user_config.h - what have I misinstalled?

720 Views
stevepye
Contributor I

java.lang.NullPointerException

     at com.freescale.mqx.configuration.editor.model.parser.Parser.fillPage(Parser.java:100)

     at com.freescale.mqx.configuration.editor.model.ModelProvider.fillPages(ModelProvider.java:59)

     at com.freescale.mqx.configuration.editor.model.ModelProvider.<init>(ModelProvider.java:31)

     at com.freescale.mqx.configuration.editor.ConfigurationEditor.getModelProvider(ConfigurationEditor.java:95)

     at com.freescale.mqx.configuration.editor.ConfigurationEditor.createPages(ConfigurationEditor.java:116)

     at org.eclipse.ui.part.MultiPageEditorPart.createPartControl(MultiPageEditorPart.java:358)

0 Kudos
3 Replies

571 Views
soledad
NXP Employee
NXP Employee

Hi Steve Pye

Could you please provide a little more information about this issue?

Are you using CodeWarrior, IAR, KDS, or another IDE?

Which board are you using?

Could please provide a screenshot of this issue?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

571 Views
stevepye
Contributor I

Hi Soledad,

Okay, recovered from project troubles. Fortunately I had the faulty-project

in another Workspace so I was able to re-import it.

I've attached a screen-shot after I double-clicked on user_config.h in my

BSP project.

One other symptom, perhaps: I no longer have 'BSP Cloning Wizard' as an

'MQX Tools' menu option. Do I need to reinstall MQX?

Thanks,

Steve.

0 Kudos

571 Views
stevepye
Contributor I

I'm using CodeWarrior 10.6. I'm using a board we developed ourself based on

a Kinetis K20.

I can't get a screen-shot because CodeWarrior Processor Expert

Code-Generator has just mucked up my bsp_Xxxx project and I'm no longer able

to open the project. The Processor Expert was complaining about not being

able to write some .h files to folder PDD\*.h. After exiting CodeWarrior

and then re-opening, the Project file is no longer openable, and it's kind

of an important project that includes all the MQX and BSP stuff.

0 Kudos