Hi-
My board is based on MK20DX128VFM5 and powered my MQX4.1.1.
Testing low power mode using VLPR by following demo code from Freescale_MQX_4_1\mqx\examples\lowpower. What I can see is the current consumption is decreased by 20mA on entering VLPR mode. But I can't get it back to RUN mode by using MQX APIs in the demo code. Here are what I used:
enter VLPR:
_lpm_set_clock_configuration(BSP_CLOCK_CONFIGURATION_2MHZ);
_lpm_set_operation_mode (LPM_OPERATION_MODE_WAIT);
exit VLPR:
_lpm_set_operation_mode (LPM_OPERATION_MODE_RUN);
_lpm_set_clock_configuration(BSP_CLOCK_CONFIGURATION_DEFAULT);
THe code above crashed in API _lpm_set_clock_configuration(BSP_CLOCK_CONFIGURATION_DEFAULT), what is the reason for it?
How can I verify the ARM core is running at 4MHz?
Another question is, since my application enters VLPR mode immediately after power on, the IAR used can't JTAG it to load a new code in because VLPR prevents from FLASH programming. Any solution to it?
Thanks!
Hui
解決済! 解決策の投稿を見る。
Hi Sol
Thanks for your help. I worked around it by setting MCG_G2 to 0x25U (high gain to low power) so that my external crystal circuit can start oscillation again on the way back to RUN mode.
regards
Hui
some more info I just got from debugging:
My silicon SIM_SDID is 0x3012
prints on silicon is 3N86B
On resuming back to RUN mode, the processor hangs when it migrates from FBI to FBE mode in Cpu_SetMCGModePBE() of bsp_cm.c:
...
/* MCG_C1: CLKS=2,FRDIV=3,IREFS=0,IRCLKEN=0,IREFSTEN=0 */
MCG_C1 = (uint8_t)0x98U;
...
Hello,
Please check the below thread: MQX Low Power Mode: stop from wait
Let me know if this helps!!!
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sol
Thanks for your help. I worked around it by setting MCG_G2 to 0x25U (high gain to low power) so that my external crystal circuit can start oscillation again on the way back to RUN mode.
regards
Hui