MQX with MK53N512CMD10 custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX with MK53N512CMD10 custom board

Jump to solution
1,465 Views
ing_albertopc
Contributor I

Hi, I´m using a mqx project on a custom board with a MK53N512CMD10 and an external cristal of 8MHz. I try to use the proccesor expert to configure the external cristal, and got stuck on this line of code at dispatch.S file:

ASM_LABEL(no_one_to_run)

                / woohoo, idle task must be enabled, this point cannot be reachable, you have serious problem /

               b .

¿does the K53N512CMD10 with MQX support an external cristal of 8MHz?

¿How do i configure MQX to work with the external cristal of 8MHz?

¿How do i link my MXQ proyect with a bsp clon?

I'll be thankful for your help

Regards

Alberto

0 Kudos
Reply
1 Solution
440 Views
soledad
NXP Employee
NXP Employee

Hello Alberto,

I have reviewed this issue and this may helps.

The TWR-K53N512 BSP has been created for the TWR-K53N512, Rev.C schematics (SCH-26994), Rev.X3 BOM

(700-26694). This TWR-K53N512 board is populated by PK53N512CMD100. The BSP does not work for TWRK53N512

boards populated by MK53DN512CMD10 with the 4N22D mask set. A workaround is to use the

twrk60d100m BSP for this kind of TWR-K53N512 board.

I think this is the issue. Could you please try again cloning the wtrk60d100m BSP instead the twrk53?

Please let me know if this helps.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
441 Views
soledad
NXP Employee
NXP Employee

Hello Alberto,

I have reviewed this issue and this may helps.

The TWR-K53N512 BSP has been created for the TWR-K53N512, Rev.C schematics (SCH-26994), Rev.X3 BOM

(700-26694). This TWR-K53N512 board is populated by PK53N512CMD100. The BSP does not work for TWRK53N512

boards populated by MK53DN512CMD10 with the 4N22D mask set. A workaround is to use the

twrk60d100m BSP for this kind of TWR-K53N512 board.

I think this is the issue. Could you please try again cloning the wtrk60d100m BSP instead the twrk53?

Please let me know if this helps.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply