MQX Lite Support for Kl27X SOC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX Lite Support for Kl27X SOC

535 次查看
anilnadargi
Contributor II

We are using MQX Lite on MKL27Z256VMP4 SoC . We have installed GPIO driver and LP UART driver using Processor Expert.

Setup :

1. SoC MKL27Z256VMP4 .

2. GPIO Driver

3. LP UART Driver

4. MQX Lite / FreeRTOS

Observations :

1. When we run the firmware only with GPIO driver installed ,firmware is running fine with issues and we are able to toggle the GPIO pins.

2. When we try to run firmware installed the LP UART driver in the firmware along with GPIO driver , firmware get reset . After debugging enabled we found the program jumps to Reset Handler code within the boot.S file .

3. But when we changed the OS options from MQX Lite to Bare-metal , the firmware ( LP UART + GPIO ) works just fine, i.e. we are able to toggle the GPIO lines and also able to receive the data from LP UART module .

Queries :

1. Do we need to modify some memory from default settings to run RTOS for above SoC ( MKL27Z256VMP4 ).

2. Does MQX Lite and FreeRTOS supports above SoC ( MKL27Z256VMP4 ).

Thanks ,

Anil N.

0 项奖励
1 回复

303 次查看
soledad
NXP Employee
NXP Employee

Hello Anil,

MQX Lite and FreeRTOS supports the MKL27Z256VMP4. I suggest to download Kinetis® SDK v2 from the next link:

Software Development Kit for Kinetis MCUs|NXP

After download KSDK v2, you will find an example code that you can use as reference at the path:

<SDK_2.0_name_device>\boards\<nameboard>\rtos_examples\freertos_lpuart


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励