Hi everybody,
Currently I am working with HCS12 controllers and now I am going to make the big step to kinetis controllers.
I will use MK40 and MQX OS.
Currently I am trying to familiarize myself with MQX; the whole thing of RTOS is complete new for me.
I have installed MQX 4.1 and codewarrior 10.6.
I have made the following steps:
-New MQX 4.1 project
-kwikstik board
-new application
-no additional mqx libraries
-empty application
When I compile the project, the following error and warnings occur:
Error
Description | Resource | Path | Location | Type |
mingw32-make: *** No rule to make target `C:/Freescale/Freescale_MQX_4_1/lib/kwikstikk40x256.cw10gcc/debug/bsp/intflash.ld', needed by `explicit-dependencies'. Stop. | MQX_Prg1 | C/C++ Problem |
Warnings
Description | Resource | Path | Location | Type |
Invalid project path: Include path not found (C:\Freescale\Freescale_MQX_4_1\lib\kwikstikk40x256.cw10gcc\debug\bsp). | MQX_Prg1 | pathentry | Path Entry Problem | |
Invalid project path: Include path not found (C:\Freescale\Freescale_MQX_4_1\lib\kwikstikk40x256.cw10gcc\debug\bsp\Sources). | MQX_Prg1 | pathentry | Path Entry Problem | |
Invalid project path: Include path not found (C:\Freescale\Freescale_MQX_4_1\lib\kwikstikk40x256.cw10gcc\debug\bsp\Generated_Code). | MQX_Prg1 | pathentry | Path Entry Problem |
It is expected that an empty application created by wizard should work (compile).
Could anyone tell what is going wrong?
Sorry if it is silly question but the RTOS and Kinetis are complete new for me.
I have attached a screenshot and the project.
Thank you
Original Attachment has been moved to: MQX_Prg1.zip
Solved! Go to Solution.
hello Eric,
You need rebuild bsp and psp before work with a new project.
Please refer C:\Freescale\Freescale_MQX_4_1\doc\tools\cw\MQX_CW10_Getting_Started.pdf
For how to rebuild the bsp and psp.
please go to "project", "clean..." then rebuild the project.
==========================================
this answer is for you. if it helps, please click on "correct answer " button. thanks!
Best Regards ,
ZhangJun
hello Eric,
You need rebuild bsp and psp before work with a new project.
Please refer C:\Freescale\Freescale_MQX_4_1\doc\tools\cw\MQX_CW10_Getting_Started.pdf
For how to rebuild the bsp and psp.
please go to "project", "clean..." then rebuild the project.
==========================================
this answer is for you. if it helps, please click on "correct answer " button. thanks!
Best Regards ,
ZhangJun
Hi ZhangJun
I have rebuilt MQX libraries and now it works.
Thank you
Hi Eric_t d;
In addition you can check the application note attached, this app note provides information that enables developers to start a first application on Freescale MQX RTOS easily.
This may helps;)
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------