Disable console on UART with printf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable console on UART with printf

3,067 Views
aroste
Contributor IV

Hi,

I'm not sure the title is very correct. 

I use latest CW 10.4 and MQX 4.0 with a K60F120M bsp configuration.  I use the console printf for debug and redirected it to an UART (UART2 -> ttyc)  and it works fine.

So I use printf in my code to help debug and develop.  => OK

Now I reach the final steps, this UART should be used for something else so I want to completely disable the console output.

What should I do?

And what should I do with all the places I use printf now? 

Thanks and best regards

-stéphan-

0 Kudos
Reply
3 Replies

2,344 Views
stevejanisch
Contributor IV

I have always incorporated a simple Ethernet or telnet interface into my applications (of course I realize this doesn't help if you are not incorporating the Ethernet port).  Telnet is still available as a command line interface in most operating systems... including Windows (although they are making it more and more difficult to locate).

0 Kudos
Reply

2,344 Views
BielikM
Contributor III

Hi -stéphan-,

In file \mqx\source\bsp\<BOARD_NAME>\<BOARD_NAME>.h is defined BSP_DEFAULT_IO_CHANNEL. You can change it here,probably set to NULL.(also you can set this macros in user_config.h).

If you want change only app you can use function _io_set_handle() and change IO_STDOUT and IO_STDIN to NULL or other io driver. ! !

_io_set_handle(IO_STDOUT, NULL);

I hope this answer will help.

Regards,

Martin

0 Kudos
Reply

2,344 Views
DavidS
NXP Employee
NXP Employee

Hi Stephan,

Martin has best solution to disable the default io capability.

Another method would be to make modifications to the user_config.h (this is the highest level header file in the RTOS that can over ride default RTOS settings).

Simply setting all the selected BSPCFG_ENABLE(I)TTYx #defines to 0 will disable the RTOS from using a physical UART.

That doesn't resolve the printf's matter you have in your code base.

For that you can modify the PSP fio.h header and add a #define to the user_config.h to switch on and off the printf capability:

fio.h modifications:

ScreenHunter_32 Oct. 22 13.06.gif

user_config.h modification:

ScreenHunter_33 Oct. 22 13.06.gif

As always, please re-compile the RTOS when making modifications to user_config.h.

Regards,

David

0 Kudos
Reply