In the DHCP server module dhcpsrv.c, two of the service functions are empty. Shouldn't there be some processing in there? For example, DHCPSRV_service_release should place the IP address back in the pool.
解決済! 解決策の投稿を見る。
Hi Tony:
You are right, upon receipt of a DHCPRELEASE message, the server marks the network address as not allocated and retain a record of the client's initialization parameters for possible reuse. Upon receipt of a DHCPDECLINE message, the server must mark the network address as not available and should notify the local system adminstrator of a possible configuration problem.
unfortunately, these two functions are not implemented yet, and no plan to implement it in classic MQX 4.x yet. I would suggest you implement it by yourself if it is necessary.
Regards
Daniel
Hi Tony:
You are right, upon receipt of a DHCPRELEASE message, the server marks the network address as not allocated and retain a record of the client's initialization parameters for possible reuse. Upon receipt of a DHCPDECLINE message, the server must mark the network address as not available and should notify the local system adminstrator of a possible configuration problem.
unfortunately, these two functions are not implemented yet, and no plan to implement it in classic MQX 4.x yet. I would suggest you implement it by yourself if it is necessary.
Regards
Daniel
Hi Daniel,
Thanks for your reply. As I suspected, the functions are not implemented yet. I will see if I need those functions and implement them if need be.
Regards
Tony