led

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
1,038 次查看
smallyang
Contributor III

亲们我请教下,例程led我们想改两个引脚。是只用改这个数字嘛?  其他的我们需要改动嘛 ?  例子用的这个113,手册上和我们用87和88看起来是差不多的。

Dear, let me ask you, routine led we want to change two pins. Are we just gonna change this number? Do we need to change anything else? The example uses 113, which in the manual looks pretty much the same as we used 87 and 88.

smallyang_0-1712712737441.jpeg

 

smallyang_1-1712712746750.png

 

smallyang_2-1712712757534.png

smallyang_3-1712712778747.png

smallyang_4-1712712819490.jpeg

 

smallyang_5-1712712834870.png

 

 

 

0 项奖励
回复
1 解答
986 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please see the reference manual for configuration of internal flash boot:

petervlna_0-1712828189701.png

Best regards,

Peter

 

在原帖中查看解决方案

0 项奖励
回复
8 回复数
1,017 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am confused from your post.

Which microcontroller you are speaking about? Do you have a NXP EVB or your own board?

What you want to achieve? You want to change output state of specific GPIO pins? Which ones?

Best regards,

Peter

0 项奖励
回复
1,002 次查看
smallyang
Contributor III

您好,  我有个新的问题。   我想问下电路板这些引脚怎么设置才能用同调试器从jtag口下载调试呢?

Hello, I have a new question. I would like to ask how to set these pins of the circuit board to download debugging from the jtag port with the debugger?

smallyang_0-1712807363000.png

smallyang_1-1712807531058.png

 

 

 

0 项奖励
回复
987 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please see the reference manual for configuration of internal flash boot:

petervlna_0-1712828189701.png

Best regards,

Peter

 

0 项奖励
回复
970 次查看
smallyang
Contributor III

smallyang_0-1712884027748.png

 

externa. watchdog    Hello, How to remove watchdog?

 

0 项奖励
回复
982 次查看
smallyang
Contributor III

TEST = 0:

smallyang_1-1712829047075.png

 

TEST = 1  :

smallyang_0-1712829022681.png

What about the other pins?

0 项奖励
回复
983 次查看
smallyang
Contributor III

PLLCFG0 PLLCFG1  WKPCFG  TEST EVTI

0 项奖励
回复
984 次查看
smallyang
Contributor III

好的谢谢您,我用RAM也是这样配置吗 ,其他引脚呢

Ok, thank you. Do I use RAM in the same way? What about the other pins?

smallyang_0-1712828421600.png

 

smallyang_1-1712828446583.png

 

0 项奖励
回复
1,016 次查看
smallyang
Contributor III

您好,我们想把led Example_MPC5554EVB-PinToggleStationery-v0_2-CW210的gpio113改成gpio87

 

Hello, we want to change gpio113 of led Example_MPC5554EVB-PinToggleStationery- V02-CW210 to gpio87

0 项奖励
回复