[elxr] (error #21) cannot find library -lmulti

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[elxr] (error #21) cannot find library -lmulti

Jump to solution
1,690 Views
tmduybk
Contributor II

Hi,

I download Example MPC5748G Flash RW GHS614.

But when I using command line "gbuild -top MPC5748G-Flash_RW-GHS614.gpj", cmd show Error:

[elxr] (error #21) cannot find library -lmulti

I attach image of an error. Thank you !

0 Kudos
Reply
1 Solution
1,664 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

not sure what's the root cause here but the example is very simple piece of code, so you can only copy the code from main.c and add it to your project (to any IDE). No other files are needed or modified.

Regards,

Lukas

 

View solution in original post

1 Reply
1,665 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

not sure what's the root cause here but the example is very simple piece of code, so you can only copy the code from main.c and add it to your project (to any IDE). No other files are needed or modified.

Regards,

Lukas