eQADC Calibration on MPC5777C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eQADC Calibration on MPC5777C

跳至解决方案
656 次查看
berat24
Contributor III

Hello there,

I am sending gain and offset values to relevant registers for standart configuration. When I looked at the datasheet, offset and gain value registers for standart configuration is common for ADC0 and ADC1. Therefore, I am sending ofset and gain values negating BN bit on write command.

I would like to learn that sending whether these values one time is enough for taking calibrated results from ADC0 and ADC1 on eQADCA.

Sincerely. 

0 项奖励
回复
1 解答
645 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, if you consider voltage reference as clean and perfect during whole temperature drifts, then yes. But it is not too much probable.

Therefore AN2989 section 3.2 outlines run-tine calibration as an option:
https://www.nxp.com/docs/en/application-note/AN2989.pdf

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
646 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, if you consider voltage reference as clean and perfect during whole temperature drifts, then yes. But it is not too much probable.

Therefore AN2989 section 3.2 outlines run-tine calibration as an option:
https://www.nxp.com/docs/en/application-note/AN2989.pdf

 

0 项奖励
回复