eQADC Calibration on MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eQADC Calibration on MPC5777C

Jump to solution
632 Views
berat24
Contributor III

Hello there,

I am sending gain and offset values to relevant registers for standart configuration. When I looked at the datasheet, offset and gain value registers for standart configuration is common for ADC0 and ADC1. Therefore, I am sending ofset and gain values negating BN bit on write command.

I would like to learn that sending whether these values one time is enough for taking calibrated results from ADC0 and ADC1 on eQADCA.

Sincerely. 

0 Kudos
Reply
1 Solution
621 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, if you consider voltage reference as clean and perfect during whole temperature drifts, then yes. But it is not too much probable.

Therefore AN2989 section 3.2 outlines run-tine calibration as an option:
https://www.nxp.com/docs/en/application-note/AN2989.pdf

 

View solution in original post

0 Kudos
Reply
1 Reply
622 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, if you consider voltage reference as clean and perfect during whole temperature drifts, then yes. But it is not too much probable.

Therefore AN2989 section 3.2 outlines run-tine calibration as an option:
https://www.nxp.com/docs/en/application-note/AN2989.pdf

 

0 Kudos
Reply