bootloder for mpc5748G

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bootloder for mpc5748G

965 次查看
gj3526
Contributor III

Hi all,

      I'm designing a BootLoader program.The idea of the program is to receive new programs through serial ports, burn them into the FLASH according to SRC files, and then jump to execute the new program, but it doesn't run after jumping.

BootLoader:

/* define heap and stack size */

__HEAP_SIZE = DEFINED(__heap_size__) ? __heap_size__ : 0x00000000;

__STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x00001000;

/* Define FLASH */

FLASH_BASE_ADDR = DEFINED(__flash_base_addr__) ? __flash_base_addr__ :0x014C0000;

FLASH_SIZE =  DEFINED(__flash_size__) ? __flash_size__ : 1856K;

/* Define SRAM */

SRAM_BASE_ADDR = DEFINED(__sram_base_addr__) ? __sram_base_addr__ : 0x40000000;

SRAM_SIZE = DEFINED(__sram_size__) ? __sram_size__ : 768K;

MEMORY

{

    flash_rchw : org = 0x00FA0000, len = 0x4

    cpu0_reset_vec : org = 0x00FA0000+0x10, len = 0x4

    cpu1_reset_vec : org = 0x00FA0000+0x14, len = 0x4

    cpu2_reset_vec : org = 0x00FA0000+0x04, len = 0x4

 

    m_text : org = FLASH_BASE_ADDR, len = FLASH_SIZE

    m_data : org = SRAM_BASE_ADDR, len = SRAM_SIZE

}

...............................................................................................................................................................................

User APP:

/* Entry Point */

ENTRY(_start)

/* define heap and stack size */

__HEAP_SIZE = DEFINED(__heap_size__) ? __heap_size__ : 0x00000000;

__STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x00001000;

/* Define FLASH */

FLASH_BASE_ADDR = DEFINED(__flash_base_addr__) ? __flash_base_addr__ : 0x01000000;

FLASH_SIZE =  DEFINED(__flash_size__) ? __flash_size__ : 1856K;

/* Define SRAM */

SRAM_BASE_ADDR = DEFINED(__sram_base_addr__) ? __sram_base_addr__ : 0x40000000;

SRAM_SIZE = DEFINED(__sram_size__) ? __sram_size__ : 256K;

MEMORY

{

    flash_rchw : org = 0x00FA0000, len = 0x4

    cpu0_reset_vec : org = 0x00FA0000+0x10, len = 0x4

    cpu1_reset_vec : org = 0x00FA0000+0x14, len = 0x4

    cpu2_reset_vec : org = 0x00FA0000+0x04, len = 0x4

 

    m_text : org = FLASH_BASE_ADDR, len = FLASH_SIZE

    m_data : org = SRAM_BASE_ADDR, len = SRAM_SIZE

}

...............................................................................................................................................................................

Jump code

void iap_load_app(uint32_t appxaddr)

{

        INT_SYS_DisableIRQ_MC_All(LINFLEXD10_RX_IRQn);

        INT_SYS_DisableIRQ_MC_All(LINFLEXD10_TX_IRQn);

        INT_SYS_DisableIRQ_MC_All(LINFLEXD10_ERR_IRQn);

        INT_SYS_DisableIRQ_MC_All(STM0_Ch0_IRQn);

        INT_SYS_DisableIRQ_MC_All(PIT_Ch15_IRQn);

        INT_SYS_DisableIRQ_MC_All(SIUL_EIRQ_00_07_IRQn);

        INT_SYS_DisableIRQ_MC_All(SIUL_EIRQ_08_15_IRQn);

        INT_SYS_DisableIRQGlobal();

        DISABLE_INTERRUPTS(); /*disable the CPU interrupt*/

//      ((void (*)(void)) appxaddr)();

        __asm__("e_lis %r12,0x0100");

        __asm__("e_or2i %r12,0x0000");

//      __asm__("e_lwz %r0,0(%r12) ");

//      __asm__("mtlr %r0");

        __asm__("mtlr %r12");

        __asm__("se_blrl");

}

...............................................................................................................................................................................

before se_blrl

111.png

after se_blrl

pastedImage_13.png

222.png

333.png

Note:

S30900FA0000005A0002A0                   

S30900FA001001000000EB( in user APP srec file)

These two lines are not recorded in flash.

Please help to see what's wrong, or whether BootLoader's thinking is correct. Thank you very much!

 

标记 (1)
0 项奖励
回复
2 回复数

803 次查看
Frank_Jianpeng_Zhao
NXP Employee
NXP Employee

Hi, Gong jun,

From the photos attached to you, your Bootloader flash size max is 768K not 1856K.

And please check if the srec file of App programmed to flash is correct though your Bootloader?

Best Regards,

Frank

0 项奖励
回复

803 次查看
gj3526
Contributor III

Hi,Frank

Your help was very timely, and I finally found that the flash burned was different from the srec file.

and after jump need wait a moment.  thank you!

Best Regards,

gong jun

0 项奖励
回复