Program with no interrupt can not realize SPI comunicationon  continuesly and periodicaly on MPC5604C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program with no interrupt can not realize SPI comunicationon  continuesly and periodicaly on MPC5604C

1,172 Views
pengfei_ji
Fresh Out Contributor

Hi,

I want to realize SPI communication, but I have only one MPC5604C.Then I use the master mode to realize a self-send and self-recive SPI communication function,  What I want is a periodicaly send and receive funciton,but it can only self-send and self-recive one time. Following was the code without-Interrupt I modified from the CodeWarrior sample.When the functions in while() in main() is called again, the returned data is 0x0000.Can any one help find the problem in the code ? I think  we may need Interrupt, and can you provide examples using Interrupt ?

void initModesAndClks(void) {
ME.MER.R = 0x0000001D; /* Enable DRUN, RUN0, SAFE, RESET modes */
/* Initialize PLL before turning it on: */
CGM.FMPLL_CR.R = 0x02400100; /* 8 MHz xtal: Set PLL0 to 64 MHz */
ME.RUN[0].R = 0x001F0074; /* RUN0 cfg: 16MHzIRCON,OSC0ON,PLL0ON,syclk=PLL */
ME.RUNPC[1].R = 0x00000010; /* Peri. Cfg. 1 settings: only run in RUN0 mode */
ME.PCTL[4].R = 0x01; /* MPC56xxB/P/S DSPI0: select ME.RUNPC[1] */
ME.PCTL[5].R = 0x01; /* MPC56xxB/P/S DSPI1: select ME.RUNPC[1] */
ME.PCTL[68].R = 0x01; /* MPC56xxB/S SIUL: select ME.RUNPC[0] */
/* Mode Transition to enter RUN0 mode: */
ME.MCTL.R = 0x40005AF0; /* Enter RUN0 Mode & Key */
ME.MCTL.R = 0x4000A50F; /* Enter RUN0 Mode & Inverted Key */
while (ME.GS.B.S_MTRANS) {} /* Wait for mode transition to complete */
/* Note: could wait here using timer and/or I_TC IRQ */
while(ME.GS.B.S_CURRENTMODE != 4) {} /* Verify RUN0 is the current mode */
}

void initPeriClkGen(void) {
/* Use the following code as required for MPC56xxB or MPC56xxS:*/
CGM.SC_DC[1].R = 0x80; ; /* MPC56xxB/S: Enable peri set 2 sysclk divided by 1 */
}

void disableWatchdog(void) {
SWT.SR.R = 0x0000c520; /* Write keys to clear soft lock bit */
SWT.SR.R = 0x0000d928;
SWT.CR.R = 0x8000010A; /* Clear watchdog enable (WEN) */
}

void initDSPI_0(void) {
DSPI_0.MCR.R = 0x80010001; /* Configure DSPI_0 as master */
DSPI_0.CTAR[0].R = 0x780A7727; /* Configure CTAR0 */
DSPI_0.MCR.B.HALT = 0x0; /* Exit HALT mode: go from STOPPED to RUNNING state*/
SIU.PCR[13].R = 0x0604; /* MPC56xxB: Config pad as DSPI_0 SOUT output */
SIU.PCR[12].R = 0x0103; /* MPC56xxB: Config pad as DSPI_0 SIN input */
SIU.PCR[14].R = 0x0604; /* MPC56xxB: Config pad as DSPI_0 SCK output */
SIU.PCR[15].R = 0x0604; /* MPC56xxB: Config pad as DSPI_0 PCS0 output */
}


void ReadDataDSPI_0(void) {
while (DSPI_0.SR.B.RFDF != 1){} /* Wait for Receive FIFO Drain Flag = 1 */
RecDataMaster = DSPI_0.POPR.R; /* Read data received by master SPI */
DSPI_0.SR.R = 0x90020000; /* Clear TCF, RDRF, EOQ flags by writing 1 */
}

int main(void) {
initModesAndClks(); /* Initialize mode entries and system clock, PLL */
initPeriClkGen(); /* Initize peripheral clock generation for DSPIs */
disableWatchdog(); /* Disable watchdog */
initDSPI_0(); /* Initialize DSPI_0 as master SPI and init CTAR0 */

while (1) {
i++;
DSPI_0.PUSHR.R = 0x08015678; /* Transmit data from master to slave SPI with EOQ */
ReadDataDSPI_0(); /* Read data on master DSPI */
} /* Wait forever */
}

0 Kudos
Reply
1 Reply

1,101 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the code should run normally. Try to check if QOF flag is really cleared before data is stored into PUSHR.

Or try to do not use EOQ bit in command work.

BR, Petr

0 Kudos
Reply