Mcal 4.0.3 for MPC574x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mcal 4.0.3 for MPC574x

331 Views
1490491886
Contributor I

When I use the sample project, the error log shows the following statement, "  [!ERROR!]
"AUTOSAR release major version number of the Basic Software Module Description file (Gpt.epd version [!"ArReleaseMajorVersion "!]) and the Code template file (Gpt_PBcfg.c version [!"num:i($GPT_AR_RELEASE_MAJOR_VERSION_TEMPLATE)"!]) are different" 

However, the two version numbers are same.  4.0.3

 

0 Kudos
1 Reply

327 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

It looks like the example is not matching the ASR 4.0

Could you share with me the Gpt_PBcfg.c version?

Best regards,

Peter

0 Kudos