MPC5777C Address lines of EBI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5777C Address lines of EBI

跳至解决方案
691 次查看
prathapvc
Contributor III

Does MPC5777C device offers 23 address lines in non-multiplexed mode?

When non-multiplexed mode has been choosen, bits 9-30 will be reflected on the external bus D_ADD [9:30]. There is 22 address line thus maximum memory size is 8Mbytes (=2^23 because of 16-bit data bus and so D_ADD31 is not used) per chip select.

1 解答
582 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, 22 address lines. ADD31 is basically replaced by two byte strobe lines because 16-bit data port.

在原帖中查看解决方案

2 回复数
582 次查看
prathapvc
Contributor III

ok thank you

0 项奖励
回复
583 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, 22 address lines. ADD31 is basically replaced by two byte strobe lines because 16-bit data port.