MPC5775E Secure Boot Failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5775E Secure Boot Failed

238 Views
WeoWang
NXP Employee
NXP Employee

Hi Dear Colleagues,
My customer enabled secure boot on MPC5775E. Recently, their engineers tested the OTA feature, once the bootloader started to erase the app, they powered off the MCU. After that, they powered on the MCU again, the MCU started to run from the bootloader, but they found that the secure boot feature failed, CSE_SR[BOK] = 0 (normally CSE_SR[BOK] = 1, which means the secure boot is successful), according to the customer's strategy, it was not allowed for the bootloader to jump to app. By checking the registers of CSE, CSE_ECR[EC] = 0x0C (System memory error).
The customer downloaded a normal app(covers the region of bootloader and app) into the MCU, then downloaded the bootloader, used the bootloader to update the app, everything worked well.
In the customer engineer's understanding, if the OTA is interrupted, only the app is damaged, if they power on the MCU again, the bootloader should be able to update the app, but why the secure boot fails? How to prevent this issue?

0 Kudos
Reply
2 Replies

235 Views
WeoWang
NXP Employee
NXP Employee

Hi Lukas@lukaszadrapa, do you have any ideas? Thanks.

0 Kudos
Reply

202 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Please follow 00598991. Thanks.

0 Kudos
Reply