MPC5646C Power Up Sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5646C Power Up Sequence

1,131 Views
jinjingyang
NXP Employee
NXP Employee

Dear Sir,

Does this MCU MPC5646C need special power up sequence? VDD_HV applying first, or VDD_LV applying first, or don't care? Do we have a document to describe this requirement?

 

Regards,

Jason Yang

Labels (1)
3 Replies

984 Views
jinjingyang
NXP Employee
NXP Employee

Hi, Lukas,

Is it allowed to use 5V for VDD_HV, and 3.3V on ballast transistor?

Thus the power  dissipation on the ballast transistor will be less.

For this kind of case, should we power up 5V first or 3.3V first or don't  care?

Regards,

Jason Yang

0 Kudos
Reply

984 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Jason,

VDD_BV (supply of ballast transistor) can be independent of other supply voltages. It must be > 2.6V. So, 3.3V is OK. There are no power sequencing restrictions.

pastedImage_1.png

Regards,

Lukas

0 Kudos
Reply

984 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Jason,

VDD_LV is not supposed to be supplied externally on this device. VDD_LV is generated by internal voltage regulator using external ballast transistor, so there's no need to do special power up sequence.

Regards,

Lukas