IVOR1 ECC error when writing to flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IVOR1 ECC error when writing to flash

743 Views
danielnäslund
Contributor III

A write to flash goes ok, but a subsequent read triggers a machine exception and my program gets stuck in the IVOR1 exception handler.

The content of some exception handling control registers:

pastedImage_2.png

The content of C55FMC.MCR:

pastedImage_1.png

The write and reads are both 8 bytes to address 0x00f9_0000.

I'm a bit lost in the weeds here: What kind of actions would trigger a EEC error? Since it's happening consistently I assume that I must do something wrong when reading or writing to flash.

I'm still working on reduce the program down into something smaller, but I thought I might start of a question thread in case you have any immediate suggestions about what to investigate?

I'm attaching my flash-driver. Here is the write-function that calls into the driver.

bool FlashInfo::WriteSerialNumber(uint8_t const *number)
{
    if (m_State != IDLE)    // busy
        return false;

    // Start writing
    if (m_Flash.StartWriting(FlashInfo::SERIAL_NUMBER, Flash::dataFlash) == false) // command rejected
        return false;
    else
    {
        uint8_t SerialNumber[10];               // including checksum
        memcpy(SerialNumber, number, 8);
        uint16_t Checksum = CalculateChecksum(number, 8);
        SerialNumber[8] = Checksum>>8;
        SerialNumber[9] = Checksum;
        
        if (m_Flash.AddData(SerialNumber, 10) == false)
        {
            m_Flash.StopWriting();
            return false;
        }
        else
            m_Flash.Write();
    }

    m_State = WRITING_SERIAL_NUMBER;
    return true;
}

Here is the read-function:

bool FlashInfo::ReadSerialNumber(uint8_t* buffer)
{
    // Read serial number from flash
    memcpy(buffer, SERIAL_NUMBER, 8);

    // Read checksum from flash
    uint16_t Checksum = ((*SERIAL_CHECKSUM)<<8)     // high byte
        + *(SERIAL_CHECKSUM+1);                     // low byte

    if (Checksum == CalculateChecksum(buffer, 8))
        return true;
    else
        return false;
}

1 Reply

637 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, It may be several reasons, in the flash memory typically one of following reason:

- Unexpected reset during flash erase or flash program operation

- Wear out of particular flash sector = number of program/erase cycles that device’s flash is capable to withstand is exceded (in practice, real endurance is greater than specified minimum).

- Over-programming of particular flash area that is programming without erasing. It is basically software fault.

- Soft error (radiation, electro-magnetic interference, or electrical noise) during reading or executing from flash memory

- Generally it may be caused by HW fault due to damage caused by running the device out of spec whatever way.

- Finally ECC error may be intentionally generated by ECC error injection.

In your case I would guess, it could be caused by over-programming. I would try to check (debug) whether programmed area in really erased before attempt to program.