Any one got any syntax reference about “nxp_mpc5604c_1x32x128k_cflash.pcp” File or what the file Do?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any one got any syntax reference about “nxp_mpc5604c_1x32x128k_cflash.pcp” File or what the file Do?

453 Views
pengfei_ji
Contributor I

When I use S32DS IDE to program the S19 file (hardware is P&E), it shows it is useing this file:

pastedImage_1.pnghere is part of the file content(full content in appendix),what this file actual doing here?

;version 1.13, 03/30/2017, Copyright P&E Microcomputer Systems, www.pemicro.com [560x_512k_cflash]
;device NXP, MPC5604C, 1x32x128k, desc=CFlash
;begin_cs device=$00000000, length=$00080000, ram=$40000000
;end_cs
WRITE_LONG=0000C520/FFF38010/ ;Clear soft lock bit
WRITE_LONG=0000D928/FFF38010/ ;Clear soft lock bit
WRITE_LONG=FF00000A/FFF38000/ ;Disable SWT Watchdog
NO_TIMING_TEST
DOUBLE_BUFFERING
REQUIRES_PROG_VERSION=6.10/
NO_INDIVIDUAL_WRITES
NO_BASE_ADDRESS=00000000/
ADDR_RANGE=00000000/0007FFFF/00/FFFFFFF0/FFFFC000/ ; $00000000-$0007FFFF CFLASH
BLOCKING_MASK=00000007/ ;min 8 byte write
WRITE_LONG=00008000/C3F88000/ ;Reset any prior flash read errors
WRITE_LONG=A1A11111/C3F88004/ ;Send lo/mid key
WRITE_LONG=00100000/C3F88004/ ;Enable blocks for prog/erase no shadow
WRITE_LONG=C3C33333/C3F8800C/ ;Send secondarylo/mid key
WRITE_LONG=00100000/C3F8800C/ ;Enable blocks for prog/erase
;end_cs
;Low Blocks(0..5) 1-32k,2-16k,2-32k,1-128k
USER=LB Low Block Erase 1Block > /00000000/00000005/
;Mid Blocks(0..1) 2-128k
USER=MB Mid Block Erase 1Block > /00000000/00000001/

Tags (1)
0 Kudos
Reply
1 Reply

411 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

this is an internal file of S32DS which is not supposed to be modified by user.

It just clears the watchdog, it unlocks flash blocks, so they can be programmed/erased (except shadow flash) and then there's s-record which contains pre-compiled flash driver used for programming.

Regards,

Lukas

0 Kudos
Reply