A Problem about ENET Receive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A Problem about ENET Receive

936 Views
Ada_Lovelace
Contributor IV

Hi,all.

I have a problem about ENET receive,I can run the project about enet_rmii_udp. Now I want to change the ENET receive  mode, change the interrupt to polling ,but it does not work.

Does anyone know , how to config the register's bit or change the code, ENET can receive without the interrupt ?

Tags (1)
0 Kudos
Reply
2 Replies

811 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

per my understanding you should comment below 3 lines that set priority and enable RX interrupt in ENET_Driver_Rx_Init function.

INTC.PSR[211].B.PRC_SELN = 0x8; /* IRQ sent to Core 0 */
INTC.PSR[211].B.PRIN =10; /* IRQ priority = 10 (15 = highest) */


// Enable the generation of Rx frame interrupts
ENET.EIMR.B.RXF = 1;

then within main while loop you should check if EIR[RXF] flag is set and then call ENET_Rx_Handler function. For example using

if (ENET.EIR.B.RXF == 1)

{

      ENET_Rx_Handler();

}

BR, Petr

0 Kudos
Reply

811 Views
Ada_Lovelace
Contributor IV

Thank you for reply

But I still do not understand,if we don't use ENET_Rx_Handler in the vector table,close INTC.PSR[211].B.PRC_SELN = 0x8; and INTC.PSR[211].B.PRIN =10; 

I just take out the code from  ENET_Rx_Handler() and put  it in the while, make it polling,  but it can receive frames only one cycle, do I miss something?

0 Kudos
Reply