Hi guys,
I'm trying to flash the Zephyr blinky application from MCUXpresso for VSCode.
I can build the application, and I connected the OpenSDA port of the FRDM-K22F to my PC.
Afterward, I clicked on Flash Programmer in the quickstart panel. I selected the LinkServer option and hit run; then, I got the "Error: No probe detected" error message.
Thanks for your help in advance!
Solved! Go to Solution.
Hello @laszlomonda
1)Do you have any other IDEs on your PC? For example MCUXPresso IDE? KEIL? IAR?
Debug with one of them first? Just want to confirm whether the board can work well.
2) Try to update the bootloader firmware to Jlink_OpenSDA, then debug again.
About how to update bootloader, please refer to:
Quick start guide:
https://www.nxp.com/webapp/Download?colCode=FRDM-K22F-QSG
BR
Alice
Hi Alice,
On Linux, there's no device manager, but the kernel log, which shows the device:
[ 604.529584] usb 3-1.2: new full-speed USB device number 10 using xhci_hcd
[ 604.659999] usb 3-1.2: New USB device found, idVendor=0d28, idProduct=0204, bcdDevice=10.00
[ 604.660002] usb 3-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 604.660004] usb 3-1.2: Product: DAPLink CMSIS-DAP
[ 604.660005] usb 3-1.2: Manufacturer: ARM
[ 604.660006] usb 3-1.2: SerialNumber: 0231000067424e45005600034a4f002bc521000197969900
[ 604.786014] usb-storage 3-1.2:1.0: USB Mass Storage device detected
[ 604.786160] scsi host6: usb-storage 3-1.2:1.0
[ 604.797350] hid-generic 0003:0D28:0204.000C: hiddev0,hidraw1: USB HID v1.00 Device [ARM DAPLink CMSIS-DAP] on usb-0000:0e:00.3-1.2/input3
[ 604.803033] cdc_acm 3-1.2:1.1: ttyACM0: USB ACM device
[ 605.791348] scsi 6:0:0:0: Direct-Access MBED VFS 0.1 PQ: 0 ANSI: 2
[ 605.791707] sd 6:0:0:0: Attached scsi generic sg1 type 0
[ 605.792201] sd 6:0:0:0: [sdb] 131200 512-byte logical blocks: (67.2 MB/64.1 MiB)
[ 605.792389] sd 6:0:0:0: [sdb] Write Protect is off
[ 605.792392] sd 6:0:0:0: [sdb] Mode Sense: 03 00 00 00
[ 605.792544] sd 6:0:0:0: [sdb] No Caching mode page found
[ 605.792548] sd 6:0:0:0: [sdb] Assuming drive cache: write through
[ 605.814376] sd 6:0:0:0: [sdb] Attached SCSI removable disk
The virtual drive is also mounted.
I also have these udev rules set up, so there should be no permission issues.
Yet, Visual Studio Code doesn't doesn't show any debug probes.
What should be the solution?
Hello @laszlomonda
1)Do you have any other IDEs on your PC? For example MCUXPresso IDE? KEIL? IAR?
Debug with one of them first? Just want to confirm whether the board can work well.
2) Try to update the bootloader firmware to Jlink_OpenSDA, then debug again.
About how to update bootloader, please refer to:
Quick start guide:
https://www.nxp.com/webapp/Download?colCode=FRDM-K22F-QSG
BR
Alice
Hello @laszlomonda
First check device manager of your pc, confirm the debug probe is recognized,
then refer to below link to debug:
https://mcuoneclipse.com/2023/08/16/vs-code-debugging/
BR
Alice