Hi!
I have a TWRK65F180M and I'm using Kinetis Design Studio.
Without patching the tower the FS USB is not available.
In my final product I will use HS USB, so FS is not very interesting to me.
The USB CDC example project I've looked at use FS. I try to change this define to use HS instead. It does not work. What am I doing wrong? What am i missing?
I have tried with example projects dev_cdc_vcom_freeros_twrk65f180m & dev_cdc_vcom_bm_twrk65f180m.
usb_device_config.h
/*! @brief KHCI instance count */
#define USB_DEVICE_CONFIG_KHCI (0U) // Originally 1 (KHCI is FS)
/*! @brief EHCI instance count */
#define USB_DEVICE_CONFIG_EHCI (1U) // Originally 0 (EHCI is HS)
It always hangs in fsl_clock.c:
CLOCK_EnableUsbhs0PhyPllClock()
/* Wait for lock. */
while (!(USBPHY->PLL_SIC & USBPHY_PLL_SIC_PLL_LOCK_MASK))
{
// When using EHCI, I never leave this loop.
}
Background:
I am trying to use the MCUXpresso SDK to write a USB HS driver. First I tried to cherry-pick and insert in my existing project. It showed up in Windows Device Manager, ut I could not install the driver. Only get some warning about this *.inf is not compatible with x64.
Instead I tried to install via Device Manager Action->Add Legace Hardware. It seemed to install, but did not work anyways.
So, i took a step back and started to try with TWR...
已解决! 转到解答。
Solved, found a hint here: MK66 custom board, using USB1, no PLL lock.
The readme.pdf for the example states that all jumpers should be removed on J23, this is not correct... I re-added jumper from pin 1-2 and now it seems to work.
Solved, found a hint here: MK66 custom board, using USB1, no PLL lock.
The readme.pdf for the example states that all jumpers should be removed on J23, this is not correct... I re-added jumper from pin 1-2 and now it seems to work.