rt1020 fusemap programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

rt1020 fusemap programming

632 次查看
BrianHBrook
Contributor I

We have a custom rt1020 design which uses the boot config pins and the boot mode pins for gpio if they are connected to anything at all. The ocotp example from the SDK allows shadow registers to be programmed but the precise mapping of shadow registers (on page 1129 of the rt1020 manual) to the fusemap of chapter 21 is somewhat elusive. Is there an app note or some other resource that explains this more clearly?

0 项奖励
1 回复

575 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Brian,

OCOTP load and house of fuse content into shadow registers. The description of each shadow register is scattered in may field. There isn't an AN or chapter gather these information. You have to search them one by one.

Regards,

Jing

0 项奖励