SVD file needed for K64 in Jlink ozone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SVD file needed for K64 in Jlink ozone

2,492 Views
gauravpurwar
Contributor I

I am using a sagger Jlink debugger with Kinetis K64 -MK64FN1M.

using their ozone debugger i want to peripheral registers.

for that it uses a .svd file but by default it showing some registers but not all  .

it uses ARMV7  svd for that can anyone provide me a solution.

i want to see all peripherals like i2c lin port etc

kinetis-k64‌ segger jlink‌ #svd

Labels (1)
0 Kudos
3 Replies

2,044 Views
lpcxpresso_supp
NXP Employee
NXP Employee

SVD files for specific parts are supplied as part of the MCUXpresso SDK packages (MCUXpresso SDK|NXP ), which you can generate and download from http://mcuxpresso.nxp.com/

These SVD files are automatically used by our own IDE and debugger (including if you use our debugger via J-Link.

But if you wish to use the SVD file with a third party debugger, you will need to manually extract the required SVD (XML) file from the package and follow the instructions provided by the third party to make them accessible to your debugger.

Regards,

MCUXpresso IDE Support

0 Kudos

2,036 Views
silent-dawn
Contributor II

Hello,

I found all the SVD(.xml) files are used for NXP mcuxpresso IDE and they do not follow the rules of CMSIS shown in the website https://www.keil.com/pack/doc/CMSIS/SVD/html/index.html

Does NXP provides the .svd file for a specific core or a specific board? If so, could you please share a method how to get the .svd file?

Thanks.

0 Kudos

2,044 Views
aberger
Contributor V

Can you provide instructions for how to manually extract the SVD file?

0 Kudos