Relocate library functions to ITCM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Relocate library functions to ITCM

827 Views
nickwallis
Senior Contributor I

Hi,

I would like to relocate string handling library functions (e.g. strcat()) so that they are run from ITCM.

How should I do that please? I think these come from libc, my project is using Newlib.

thanks!

-Nick

0 Kudos
3 Replies

801 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) How should I do that please? I think these come from libc, my project is using Newlib.
-- It's able to make it via modifying the linker file, so I'd like to suggest you refer to the user guide of the IDE you used.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

814 Views
nickwallis
Senior Contributor I

@ZhangJennie we're using MIMXRT1062, thanks!

0 Kudos

818 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi nickwallis 

Please let us know your chip part number, thus we can assign it to the right engineer.

Thanks,

Jun Zhang

0 Kudos