I use currently the Spansion S25FL032P (4MB with 64KB sectors) . It needs to be by S25FL064L. Unfortunately the generic spifi driver does not work with that chip. Is there any way to modifiy the existing LPC18_43_SPIFI_GENERIC.cfx driver? - Where can I see, which flash parts are supported?
Information on the LPC SPIFI flash drivers can be found in section 12.2.2, "SPIFI Flash drivers" in the MCUXpresso IDE v10.1 User Guide. You can also find the sources in the Examples subdirectory of the MCUXpresso IDE installation directory.
I would expect the current version of the driver to support S25FL064 though. What exactly do you see in the debug log? (See section 16.8, "The Console View" of the IDE v10.1 User Guide for details of how to access the log and copy the text from it.)
Regards,
MCUXpresso IDE Support
Thanks for the quick support.
Looking into the project for the LPC18_43_lpcspifilib_driver.zip I found the following flash parts to be supported:
S25FL016K
S25FL032P
S25FL064P
S25FL129P 64k Sector>
S25FL129P 256k Sector
S25FL164K
S25FL256S
S25FL512S
MX25L1635E
MX25L3235E
MX25L6435E
MX25L8035E
W25Q32FV
W25Q64FV
W25Q80BV
Thus the S25FL064P is supported, but the successor S25FL064L is not. The P version is deprecated. Cypress is recommending to use the L version instead.
I tried already to recompile the SPIFI driver with exchanging JEDEC Ids but it doesn't seem to work so straightforward.
best regards
-Otto Witte
Von: lpcxpresso_support
Gesendet: Donnerstag, 25. Januar 2018 16:52
An: Franz-Otto Witte <otto.witte@teconcept.de>
Betreff: Re: - Re: LCP4370 SPIFI support
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
Re: LCP4370 SPIFI support
reply from LPCX support <https://community.nxp.com/people/lpcxpresso_support?et=watches.email.thread> in MCUXpresso IDE - View the full discussion <https://community.nxp.com/message/981068?commentID=981068&et=watches.email.thread#comment-981068>
Hi Otto,
From a brief look at the datasheet, the ID bytes for the new SPIFI definition node should begin like this.
/* Add support for S25FL064L */
{
static const SPIFI_DEVICE_DATA_T pData = {
"S25FL064L",
{{0x01, 0x60, 0x17}, 0, {0}}, /* JEDEC ID, extCount, ext data */
...
Assuming this is what you have done, please can you let us know the behavour of the flash driver for the following options:
1 - a mass erase (this can be captured using the GUI flash programmer)
2 - a program operation (this can be captured using the debug log)
Also, it would be a good to test whether you can read values from the device (in the debugger memory editor) at 0x14000000. The device should be delivered erase, so should return 0xFF for each byte.
If this continues to fail, then I would next compare the config and status registers for the two parts.
Unfortunately, we currently do not have this particular device available for local testing.
Yours,
MCUXpresso IDE Support
Hi again
A look in the data sheet revealed that the clock setting were the problem - with these settings the spifi driver works also with the S25FL064L
#define SPIFI_DEVICE_S25FL064L 0 /**< Enables Cypress S25FL064L device */
#if SPIFI_DEVICE_ALL || SPIFI_DEVICE_S25FL064L
/* Add support for S25FL064L */
{
static const SPIFI_DEVICE_DATA_T pData = {
"S25FL064L",
{{0x01, 0x60, 0x17}, 0, }, /* JEDEC ID, extCount, ext data */
(SPIFI_CAP_DUAL_READ | SPIFI_CAP_QUAD_READ | SPIFI_CAP_QUAD_WRITE | SPIFI_CAP_FULLLOCK |
SPIFI_CAP_NOBLOCK), /* Capabilities */
128, /* # of blocks */
0x10000, /* block size */
0, /* # of sub-blocks (Does NOT support full sub-block erase) */
0, /* sub-block size 0x1000 */
256, /* page size */
MAX_SINGLE_READ, /* max single read bytes */
54, /* max clock rate in MHz */
108, /* max read clock rate in MHz */
108, /* max high speed read clock rate in MHz */
108, /* max program clock rate in MHz */
108, /* max high speed program clock rate in MHz */
FX_spifiDeviceDataInitDeinit, /* (Fx Id) use generic deviceInit / deInit */
FX_spifiDeviceDataClearStatusS25FL032P, /* (Fx Id) has persistent bits in status register */
FX_spifiDeviceDataGetStatusS25FL032P, /* (Fx Id) getStatus */
FX_spifiDeviceDataSetStatusS25FL032P, /* (Fx Id) setStatus */
FX_spifiDeviceDataSetOptsQuadModeBit9, /* (Fx Id) to set/clr options */
FX_spifiDeviceInitReadCommand, /* (Fx Id) to get memoryMode Cmd */
FX_spifiDeviceInitWriteCommand /* (Fx Id) to get program Cmd */
};
static SPIFI_DEV_NODE_T data; /* Create persistent node */
data.pDevData = &pData; /* save the data in the node */
spifiDevRegister(&devFamily, &data); /* Register the new device */
}
#endif
Thanks for your good support.
-Otto
Von: lpcxpresso_support
Gesendet: Donnerstag, 25. Januar 2018 17:31
An: Franz-Otto Witte <otto.witte@teconcept.de>
Betreff: Re: - Re: LCP4370 SPIFI support
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
Re: LCP4370 SPIFI support
reply from LPCX support <https://community.nxp.com/people/lpcxpresso_support?et=watches.email.thread> in MCUXpresso IDE - View the full discussion <https://community.nxp.com/message/981028?commentID=981028&et=watches.email.thread#comment-981028>