Goodday,
Does anybody know where I can find (change) the file with the output-pins for connecting the Red, Blue, Green and White to the JN5189?
I'm developping an JN-AN-1218-Zigbee-3-0-Light-Bulb with MCUXpresso 11.9 and installed SDK JN5189DK6
Hello,
Please refer to board.h (JN-AN-1244\Common_Light\Source\board_k32w0\board.h).
Also, you would need to check the JN-AN-1244\Common_Light\Source\DriverBulb\DriverBulb_JN518x.c.
Regards,
Ricardo
@Ricardo_Zamora Thank you for your reply.
I've looked in the files you mentioned. But it is unclear to me wich GPIO are beeing used for the Red Green Blue White Leds..
Hello,
There are some defines on the mentioned files. For example, BOARD_LED_RED1_GPIO_PORT, BOARD_LED_RED1_GPIO_PIN, LED_RED1_INIT, LED_RED1_ON, LED_RED1_OFF.
Regards,
Ricardo
Thank you for your reply.
I've seen the lines you refer to.
But my question is: which pins do they relate to?
It only refers to Red1 and Red2 on what I believe is a development board.
Doesn't there have to be: Red, Green, Blue and White? With the specified pins?
Nobody?
Do NXP employees know this?