Defective MCUXpresso Import SDK Display Windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Defective MCUXpresso Import SDK Display Windows

784 Views
mignacio
Contributor III

Hi,

I just downloaded and installed MCUXpresso latest version v11.2.0 on my Windows 10 64-bit PC.

I also downloaded a couple of SDKs to boot.

Inside MCUXpress, I did Import SDK examples...  Selected the example I like then click "next" buttons.

Please refer to the 2 attached screenshots:

For some reason, it looks like the window graphics are out of wack because there seems to be some portions that are

   "garbage" or hidden and I can't scroll up or down to see what else should be displayed within those sub-windows.

Does anyone know what's going on?

Thanks,

MI

0 Kudos
2 Replies

740 Views
converse
Senior Contributor V

This looks like a problem with the (Windows) display driver for your graphics card. Make sure Windows is up to date and you are using the latest version of the driver for your graphics card.

0 Kudos

739 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi M

I checked MCUXpresso IDE v10.2.0 on my computer, 64bit win10, I didn't see this issue.

I suggest you test it with creating a new workspace. see how it works.

If problem persists, please reinstall it to another install path, check again.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos