What tool-set for K22F ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What tool-set for K22F ?

1,043 Views
stf
Contributor I

I got an FRDM-K22F. Went to tools page looking for an SDK for this family. Found:

1. MCUXpressoSDK

2. MCUXpressoIDE

3. LPCXpressoIDE

4. Kinetis Design Studio

and maybe others. 

 

It is a total mess. I cannot find a word of explanation what are these and why so many and what differences and how to choose. 

To be honest I tried them all before writing this note. None of these is able to connect to my board. Maybe if I invest days trying. Problem I do not have time.

Please help and point the tool I should use.

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

950 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Stephan,

I'll be happy to clarify these for you. First you will need MCUXpresso IDE (LPCXpresso IDE is the older version of this and therefore no longer recommended) this is the software environment that will allow you to create projects of your own or begin from an example and make the modifications you need.

The MCUXpresso SDK is a package of drivers already made with different examples and demos that you may use as a reference or as a base for your application. This means that SDK can be imported into MCUXpresso IDE.

Lastly Kinetis Design Studio is an even older version so I do not recommend to start with this.

This is the MCUXpresso IDE:

pastedImage_1.png

You can download the SDK on the mcuxpresso sdk website -> select the board:

pastedImage_2.png

Then select build mcuxpresso sdk then on the new page that opens select add software component

pastedImage_5.png

In the dropdown menu that opens it will allow you to select all:

pastedImage_7.png

Next press download SDK and the zip folder that gets downloaded can be dragged and dropped into the MCUXpresso IDE in the Installed SDKs section.

pastedImage_8.png

Once it is imported, on the left hand side in the "Quickstart panel" you can click on import sdk examples and select your board.

pastedImage_14.png

Next you will be presented with many examples. I recommend to start with the helloworld demo. Please make sure to select UART(so you can see the output in a serial terminal like TeraTerm). Then click finish

pastedImage_16.png

Plug in your board on the open SDA usb port, then build the project by clicking on the hammer symbol on the top part and the once it is built press the blue bug to begin debugging.

pastedImage_18.png

In debug mode the tools will open to run the demo completly, do step by step, restart or pause if necessary.

I hope this information helps you and if you come across anything else, please don't hesitate to ask.

Have a great day!

Sabina

0 Kudos
Reply

950 Views
stf
Contributor I

Installed the IDE and SDK as instructed. Loaded example bubble. Builds fine - 0 errors. Hit the blue bug and got error.

Please see the attached files.

Please advise how to fix it.

Many thanks.SWDconfig.JPG

Executing flash operation 'Program' (Program file into flash: frdmk22f_bubble.axf) - Wed Dec 04 11:55:02 PST 2019
Checking MCU info...
Scanning for targets...
Executing flash action...
MCUXpresso IDE RedlinkMulti Driver v11.0 (Aug 27 2019 16:46:33 - crt_emu_cm_redlink.exe build 22)
( 0) Reading remote configuration
Wc(03). No cache support.
Found part description in XML file MK22F51212_internal.xml
( 5) Remote configuration complete
Reconnected to existing LinkServer process.
============= SCRIPT: kinetisconnect.scp =============
Kinetis Connect Script
Connecting to Probe Index = 1
This probe = 1
This TAP = 0
This core = 0
DpID = 2BA01477
Assert NRESET
Reset pin state: 00
Power up Debug
MDM-AP APID: 0x001C0000
MDM-AP System Reset/Hold Reset/Debug Request
MDM-AP Control: 0x00000000
MDM-AP Status (Flash Ready) : 0x00000036
Part is secured
Mass Erase Required
============= END SCRIPT =============================
Probe Firmware: DAPLink CMSIS-DAP (ARM)
Serial Number: 0231000032254e450034800bb529004d3f31000097969900
VID:PID: 0D28:0204
USB Path: \\?\hid#vid_0d28&pid_0204&mi_03#7&1b1dc830&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Using memory from core 0 after searching for a good core
Using memory from core 0 after searching for a good core
Using memory from core 0 after searching for a good core
connection failed - Nn(05). Wire ACK Fault in DAP access.. Retrying
Using memory from core 0 after searching for a good core
Using memory from core 0 after searching for a good core
Using memory from core 0 after searching for a good core
Failed on connect: Nn(05). Wire ACK Fault in DAP access
Connected&Reset. Was: NotConnected. DpID: 2BA01477. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 0
Debug bus selected: MemAp 0
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
(100) Target Connection Failed
error closing down debug session - Nn(05). Wire ACK Fault in DAP access
Unable to perform operation!
Command failed with exit code 1

0 Kudos
Reply

950 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Stephan,

If you are using the FRDM-K22 board you will see that it has two usb ports. One is for usb directly however this does not allow you to debug(you would have to use an external debugger to program).

The other usb port will say SDA in small letters. This one is the one that will be recognized at the point in your image that you posted above. Please try the other port and try again.

Once recognized you should see an option in the same window then press ok.

Let me know if this results successful for you.

Best Regards,

Sabina

0 Kudos
Reply

950 Views
Sabina_Bruce
NXP Employee
NXP Employee

I forgot to mention. In the overview page of the evaluation board there is a get started button.

pastedImage_1.png

This will redirect you to a step by step guide of how to get it up and running.

0 Kudos
Reply

950 Views
stf
Contributor I

Thank you much Sabina.

0 Kudos
Reply