WHEN I TRIED TO COMPILE THE SOURCE CODE OF IMX6ULLEVK ,THE BELOW ERROR WAS THROWN.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WHEN I TRIED TO COMPILE THE SOURCE CODE OF IMX6ULLEVK ,THE BELOW ERROR WAS THROWN.

882件の閲覧回数
devika_ramesh
Contributor I

Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 1 CROSS_COMPILE=arm-poky-linux-gnueabi- PLATFORM= INCLUDE=-I/home/vvdn/Projects/tixu_mx8m/tixu_mx7d/imx-yocto-bsp/build-6y/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/imx-lib/1_git-r0/recipe-sysroot/usr/include/imx all
| make -C pxp all
| make[1]: Entering directory '/home/vvdn/Projects/tixu_mx8m/tixu_mx7d/imx-yocto-bsp/build-6y/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/imx-lib/1_git-r0/git/pxp'
| arm-poky-linux-gnueabi-gcc -march=armv7ve -marm -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a7 --sysroot=/home/vvdn/Projects/tixu_mx8m/tixu_mx7d/imx-yocto-bsp/build-6y/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/imx-lib/1_git-r0/recipe-sysroot -D -I/home/vvdn/Projects/tixu_mx8m/tixu_mx7d/imx-yocto-bsp/build-6y/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/imx-lib/1_git-r0/recipe-sysroot/usr/include/imx -Wall -fPIC -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/home/vvdn/Projects/tixu_mx8m/tixu_mx7d/imx-yocto-bsp/build-6y/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/imx-lib/1_git-r0=/usr/src/debug/imx-lib/1_git-r0 -fdebug-prefix-map=/home/vvdn/Projects/tixu_mx8m/tixu_mx7d/imx-yocto-bsp/build-6y/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/imx-lib/1_git-r0/recipe-sysroot= -fdebug-prefix-map=/home/vvdn/Projects/tixu_mx8m/tixu_mx7d/imx-yocto-bsp/build-6y/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/imx-lib/1_git-r0/recipe-sysroot-native= -c pxp_lib.c -o pxp_lib.o
| <command-line>:0:1: error: macro names must be identifiers
| In file included from pxp_lib.c:26:0:
| pxp_lib.h:19:10: fatal error: linux/pxp_device.h: No such file or directory
| #include <linux/pxp_device.h>
| ^~~~~~~~~~~~~~~~~~~~
| compilation terminated.
| Makefile:32: recipe for target 'pxp_lib.o' failed
| make[1]: *** [pxp_lib.o] Error 1
| make[1]: Leaving directory '/home/vvdn/Projects/tixu_mx8m/tixu_mx7d/imx-yocto-bsp/build-6y/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/imx-lib/1_git-r0/git/pxp'
| Makefile:17: recipe for target 'pxp' failed
| make: *** [pxp] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/vvdn/Projects/tixu_mx8m/tixu_mx7d/imx-yocto-bsp/build-6y/tmp/work/cortexa7hf-neon-mx6ul-poky-linux-gnueabi/imx-lib/1_git-r0/temp/log.do_compile.7294)

0 件の賞賛
返信
1 返信

823件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello devika,

Try to erase all the build and rebuild the yocto again, this error is due to multiple yocto installed on the system.

Regards

0 件の賞賛
返信