MCUXpresso iMX Run Free mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso iMX Run Free mode

884 Views
variable_andrew
Senior Contributor I

In other NXP/Freescale processors - I remember being able to download code to the processor via the Eclipse based IDE - and then run free / detach. 

Currently this option ("Disconnect") appears to be grayed out in MCUXpresso Run dropdown when running. 

How would one try running their application and then disconnecting the debugger (and debugger cable) from the hardware while the app continues running?

Labels (1)
3 Replies

740 Views
BlackNight
NXP Employee
NXP Employee

Hi Andrew,

I assume you are using LinkServer as connection?

You can configure this in the launch/debug configuration:

pastedImage_1.png

See as well MCUXpresso IDE: Terminate and Disconnect a Debug Session | MCU on Eclipse

I hope this helps,

Erich

740 Views
variable_andrew
Senior Contributor I

Thanks for the link, Erich. 
I am using the LinkServer as you said, and settings are already set to the necessary Disconnect Behavior - but the problem is that disconnect is grayed out when running, so this is what the debugger looks like while actively running:

Screen Shot 2019-08-12 at 10.35.58 AM.png

As noted in the Terminate and Disconnect link you shared, the square red button I am able to press does this:

The expected behaviour is to stop the target under debug and disconnect

But the disconnect button is disabled. 

How might I enable the disconnect button so I can disconnect?

This is what the debugger settings look like for me:

Screen Shot 2019-08-12 at 10.27.17 AM.png

0 Kudos
Reply

740 Views
variable_andrew
Senior Contributor I

Additionally - the behavior is the same for both hardware debug interfaces I've tested:

1. Connecting directly to the RT1015EVK's onboard USB-debugger

2. Connecting to the EVK's JTAG pins (J55) via an external LPC-Link2 board

0 Kudos
Reply