IMXRT 1050 EVKB Flashing error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT 1050 EVKB Flashing error

730 Views
rizwanm
Contributor II

Hi ,

Am using IMXRT 1050 KVKB
Application : emWIN
Compiler : MCUxpresso

I generated (.sb) file using MCUXpresso file size is 2 MB
using MFG Tool if i flash our IMXRT EVKB it is not flashing and showing errror in MFG_LOG file 

" "description" : "10203 (0x27DB) kStatusMemoryCumulativeWrite",

"ModuleID[2] LevelID[10]: CmdOperation[0], current command executed failed, so SetEvent(hDevCanDeleteEvent)"

Currently am flashing in Hyper flash size of hyper flash in board is 32MB.


  i have attached MFG Error picture and log file

Thanks in advance for your reply.

Regards,

Rizwan M

0 Kudos
1 Reply

502 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Rizwan M,

What about your version of SDK and DAP-LINK ? You can refer to the below thread to check:

Programming i.MXRT with MCUXpresso IDE and BOOT 

And then use the latest SDK and DAP-link try again. Using steps the DOC list:

3. Using MFGTool program with Boot .

From the SDK2.3.1, projects and its generated *.bin file include XIP files that add this information to the project,

so we can use MFG directly flash it to external flash .

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos