SWO is Serial Wire output, it is a debug interface of Cortec-M3 and M4 core. The SWO Trace provide access to the memory of a running target without needing to interrupt target. It just requires one extra pin from MCU in addition to the standard SWD connection. It is easy to send debug information. If want to know more detail about SWO Trace, you can have a look at <MCUXpresso_IDE_SWO_Trace> .
The document of <MCUXpresso_IDE_SWO_Trace> has describe SWO Trace function in detail, so in my article , I just demonstrate the steps using SWO Trace on MCUXpresso IDE, based on LPCXpresso54114 board.
- Requirements:
MCUXpresso IDE v10.2.1 or later
MCUXpresso SDK v2.4.1 for LPC54114
LPCXpresso54114 development board
micro USB cable
Personal Computer
- Mainly
Using SWO Trace Based on NEW SDK Project and SDK Demo
3.1 Using SWO Trace Based on NEW SDK Project
Step1. Enable “Redirect printf/scanf to ITM”/Add “retarget_itm.c”
Step2. Enable SWO Pin
Step3. Enable SWO Trace clock
Step4. Add Code to Send Text
Step5. Download project
Step6. Configure MCUxpresso IDE
3.2 Using SWO Trace Based on SDK Demo
BR
Alice